This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bugs in VICP signal processing library?



Dears,

I have the question about VICP signal processing library. It seems there are 2
bugs in library's source code. Could anyone confirm the bugs?

I wrote two programs to invoke the VICP signal processing library's API
CPIS_colorSpcConv(). My first program runs smoothly but the second one always
gets the return code -1 with CPIS_errorno = 5 (CPIS_NOSUPPORTDIM_ERROR).

When I traced into CPIS_colorSpcConv(), I found the there is an abnormal array
access in function _CPIS_sizeof() (in file _cpisCore.c).
Here is the excert of the function _CPIS_sizeof():        
   
01:  Int16 _CPIS_sizeof(CPIS_Format format){
02:  
03:  Uint16 trueFormat, alphaOn;
04:   
05:  trueFormat= format & ~CPIS_ALPHA;
06:  alphaOn= format & CPIS_ALPHA;
07:   
08:  if (alphaOn && trueFormat== CPIS_RGB_888)
09:   return 4;
00:  else
11:   return (_CPIS2VICP_sizeOfFormat[trueFormat - CPIS_YUV_422IBE]);
12:   
13:  }

and the array _CPIS2VICP_sizeOfFormat[] is defined as (in file _cpisCore.c):

14: static Int16 _CPIS2VICP_sizeOfFormat[]= { 2, 2, 2, 2, 2, 3, 3, 3, 1, 1, 2,
15:              4, 8, 1, 2, 4, 8, -8, 1, 2, 4, 8, 2, 4, 8};

[bug1] (line 11) The array index (trueFormat - CPIS_YUV_422IBE) becomes
negative when trueFormat = CPIS_RGB_P or CPIS_YUV_444P. (the value of enum
CPIS_RGB_P, CPIS_YUV_444P and CPIS_YUV_422IB is 5, 1 and 7, respectively.
Note that the user guide said that CPIS_RGB_P or CPIS_YUV_444P are the native
format in function CPIS_colorSpcConv().)

[bug2] (line 14) Why there is a negative entry in the arrary
        _CPIS2VICP_sizeOfFormatat[]?

I observed that my first program has the good luck to get the valid value when
accessing the data outside the array. However, my second program which always
returns error code should be the normal case.

The VICP Signal Processing Library I used is from
VisionMid_embeddedVisionFramework, version 0.6

-------------------------------------------------------------------------.
For addition information about this question, here is the code snippet to
invoking CPIS_colorSpcConv() in my two programs.

100:   // To perform RGB to YUV conversion
101:   base.srcFormat[0] = CPIS_RGB_P;
102:   base.srcBuf[0].ptr = img_in;
103:   base.srcBuf[0].stride = img_width;
104:   base.srcBuf[1].ptr = base_param.srcBuf[0].ptr + img_width * img_height;
105:   base.srcBuf[1].stride = img_width;
106:   base.srcBuf[2].ptr = base_param.srcBuf[1].ptr + img_width * img_height;
107:   base.srcBuf[2].stride = img_width;
108:  
109:   base.dstFormat[0] = CPIS_YUV_444P;
110:   base.dstBuf[0].ptr = img_out;
111:   base.dstBuf[0].stride = img_width;
112:   base.dstBuf[1].ptr = base_param.dstBuf[0].ptr + img_width * img_height;
113:   base.dstBuf[1].stride = img_width;
114:   base.dstBuf[2].ptr = base_param.dstBuf[1].ptr + img_width * img_height;
115:   base.dstBuf[2].stride = img_width;
116:  
117:   base.roiSize.width = img_width;
118:   base.roiSize.height = img_height;
119:  
120:   base.procBlockSize.width = 16;
121:   base.procBlockSize.height = 16; 
122:  
123:   // function specific parameter 1 assignment
124:   for(i=0; i<9; i++)
125:   {
126:       param.matrix[i] = (Int16)(rgb2yuv_matrix[i] * 32768.0);
127:   }
128:   param.qShift = 15 ;
129:   param.preOffset[0] = 0;
130:   param.preOffset[1] = 0;
131:   param.preOffset[2] = 0;
132:   param.postOffset[0] = 0;
133:   param.postOffset[1] = 128;
134:   param.postOffset[2] = 128;
135:   param.signedInput[0] = 0;
136:   param.signedInput[1] = 0;
137:   param.signedInput[2] = 0;
138:   param.signedOutput[0] = 0;
139:   param.signedOutput[1] = 1;
140:   param.signedOutput[2] = 1;
141:   param.colorDsMode = CPIS_DS_NONE;
142:  
143:   ret_code = CPIS_colorSpcConv(&handle, &base &spec, CPIS_ASYNC);    

  • Hello Arthur,

    You are correct about [bug1], it is indeed a bug. Thanks for reporting it. I have attached the corrected _cpisCore.c.txt file. Rename it to _cpisCore.c and use it to rebuild the library cpis_core.aem3 .

    Regarding [bug2], it is not a bug. Actually negative number is used to express inverse of the number. So -8 means -1/8, which is the size of CPIS_1BIT .

    /* ======================================================================== */
    /*  TEXAS INSTRUMENTS, INC.                                                 */
    /*                                                                          */
    /*  VICP  Signal Processing Library                                         */
    /*                                                                          */
    /*  This library contains proprietary intellectual property of Texas        */
    /*  Instruments, Inc.  The library and its source code are protected by     */
    /*  various copyrights, and portions may also be protected by patents or    */
    /*  other legal protections.                                                */
    /*                                                                          */
    /*  This software is licensed for use with Texas Instruments TMS320         */
    /*  family DSPs.  This license was provided to you prior to installing      */
    /*  the software.  You may review this license by consulting the file       */
    /*  TI_license.PDF which accompanies the files in this library.             */
    /*                                                                          */
    /* ------------------------------------------------------------------------ */
    /*                                                                          */
    /*     NAME                                                                 */
    /*        _imgproclib.c -- imgproc module                                   */
    /*                                                                          */
    /*     DESCRIPTION                                                          */
    /*         This file implements interface functions with IP_run library     */
    /*                                                                          */
    /*     REV                                                                  */
    /*        version 0.0.2:  3rd March, 2009                                   */
    /*        Added _CPIS_updateSrcDstPtr                                       */
    /*                                                                          */
    /*        version 0.0.1:  Feb 9th, 2009                                     */
    /*        Initial version                                                   */
    /*                                                                          */
    /* ------------------------------------------------------------------------ */
    /*            Copyright (c) 2008 Texas Instruments, Incorporated.           */
    /*                           All Rights Reserved.                           */
    /* ======================================================================== */
    
    //#define _BENCHMARK_VICP
    
    /* Include the lib interface header files */
    #include "cpisCore.h"
    #include "_cpisCore.h"
    #include "cpisSched.h"
    #include "cpisCompu.h"
    #include "_cpis_utils.h"
    #include <tistdtypes.h>
    
    extern Uint8 _CPIS_demoMode;
    
    static Uint16 _CPIS2VICP_inputFormat[]= { IMXTYPE_BYTE, IMXTYPE_SHORT, IMXTYPE_LONG, 0, IMXTYPE_UBYTE, IMXTYPE_USHORT, \
                                           IMXTYPE_ULONG, 0, 0, 0, IMXTYPE_BYTE, IMXTYPE_SHORT, IMXTYPE_LONG, IMXTYPE_UBYTE, IMXTYPE_USHORT, IMXTYPE_ULONG};
    
    static Uint16 _CPIS2VICP_outputFormat[]= { IMXOTYPE_BYTE, IMXOTYPE_SHORT, IMXOTYPE_LONG, 0, IMXOTYPE_BYTE, IMXOTYPE_SHORT, \
                                           IMXOTYPE_LONG, 0, 0, 0, IMXOTYPE_BYTE, IMXOTYPE_SHORT, IMXOTYPE_LONG, IMXOTYPE_BYTE, IMXOTYPE_SHORT, IMXOTYPE_LONG};
    
    static Int16 _CPIS2VICP_sizeOfFormat[]= { 2, 2, 3, 2, 2, 3, 2, 2, 2, 2, 2, 2, 3, 3, 3, 1, 1, 2, 4, 8, 1, 2, 4, 8, -8, 1, 2, 4, 8, 2, 4, 8};
    
    Int32 _CPIS_genericCall(
     CPIS_Handle *handle,
     CPIS_BaseParms *base,
     void *params,
     CPIS_ExecType execType,
     CPIS_FuncStruct *funcStruct
    ){
    
      Uint32 maxBlockSize;
      Uint16 smallestDataSize;
    
      CHECK_INIT
      
      CPIS_obj.ipRunTab[0].functions= *funcStruct;
    
      if ((*funcStruct->checkFunc)(base, params)==-1)
       return -1;
      
    
      /* If functions that compute best block width and block height are defined */
      if (funcStruct->getMaxBlockSizeFunc && funcStruct->getBlockDimFunc) {
          /* If processing block width or height is 0 then it means API has to figure out
                 optimum block dimensions by calling (*funcStruct->getBlockDimFunc)
                 otherwise it calls (*funcStruct->getMaxBlockSizeFunc) to get the value maxBlockSize and smallestDataSize
                 which will be used by _CPIS_isBlockDimValid() to verify whether the passed values are valid.
           */
          if (base->procBlockSize.width== 0 || base->procBlockSize.height== 0) {
              if ((*funcStruct->getBlockDimFunc)(base, params, &base->procBlockSize.width, &base->procBlockSize.height)== -1) {
                  CPIS_errno= CPIS_NOSUPPORTDIM_ERROR;
                  return -1;
              }
          }
          else {
              (*funcStruct->getMaxBlockSizeFunc)(base, params, &maxBlockSize, &smallestDataSize);
    
              /* Validate the block dimension */
              if (_CPIS_isBlockDimValid(base, _CPIS_alignWithDMA2(4, smallestDataSize), maxBlockSize)== -1){
                  CPIS_errno= CPIS_NOSUPPORTDIM_ERROR;
                  return -1;
              }
          }
      }
    
      CPIS_obj.lock(CPIS_obj.lockArg);
      
      if (_CPIS_setFirst(&CPIS_obj.ipRunTab[0])== -1) {
        CPIS_obj.unlock(CPIS_obj.unlockArg);
        return -1;
        }
    
      if (funcStruct->setDmaInFunc) {
        if ((*funcStruct->setDmaInFunc)(&CPIS_obj.ipRunTab[0], base, params)==-1){
         CPIS_obj.unlock(CPIS_obj.unlockArg);
         return -1;
         }
        }
      else {
        if (_CPIS_setDmaInTransfers(&CPIS_obj.ipRunTab[0], base, funcStruct->arg)==-1){
         CPIS_obj.unlock(CPIS_obj.unlockArg);
         return -1;
         }
        }
    
      if ((*funcStruct->procFunc)(&CPIS_obj.ipRunTab[0], base, params)==-1){
         CPIS_obj.unlock(CPIS_obj.unlockArg);
         return -1;
        }
    
      if (funcStruct->setDmaOutFunc) {
        if ((*funcStruct->setDmaOutFunc)(&CPIS_obj.ipRunTab[0], base, params)==-1){
         CPIS_obj.unlock(CPIS_obj.unlockArg);
         return -1;
         }
        }
      else {
       if (_CPIS_setDmaOutTransfers(&CPIS_obj.ipRunTab[0], base, funcStruct->arg)==-1){
         CPIS_obj.unlock(CPIS_obj.unlockArg);
         return -1;
        }
      }
    
      /* if not single block, check whether the DMA settings meet constraints such as alignment */
      if (CPIS_obj.ipRunTab[0].singleBlockProcessing!= 1) {
          if(_CPIS_validateDMAconstraints(&CPIS_obj.ipRunTab[0])== -1){
              CPIS_obj.unlock(CPIS_obj.unlockArg);
              return -1;
          }
      }
    
      if (_CPIS_setLast(&CPIS_obj.ipRunTab[0], execType)== -1){
         CPIS_obj.unlock(CPIS_obj.unlockArg);
         return -1;
        }
        
      if (execType== CPIS_SYNC) {
    #if !defined(_4MACS) || defined(_SIMCOP)
        CPIS_start(NULL);
        CPIS_wait(NULL);
    #endif
        CPIS_delete(&CPIS_obj.ipRunTab[0]);
        *handle= NULL;
        }
      else {
        *handle= &CPIS_obj.ipRunTab[0];
      }
     
      return 0;
    
    }
    
    void _CPIS_dummyVicpLock(void*dummy){
      return;
    }
    
    void _CPIS_dummyVicpUnlock(void*dummy){
      return;
    }
    
    
    Int32 _CPIS_setDmaInTransfers(CPIS_IpRun *ipRun, CPIS_BaseParms *base, CPIS_Arg *arg){
    
      /* This Dma structures are used to pass information about dma transfers to IP_RUN library */
      Int32 dmaIdx;
      IP_run *ipRunObj;
      Uint16 trueSrcFormat, alphaOn;
      Int32 oldScaleFactor; 
      Uint16 roundBlockWidth; 
      Uint32 ddrOfstNextBlock, ddrOfstNextBlockRow;
      Uint16 numHorzBlocks, numVertBlocks;
      CPIS_Arg defArg;
    
      Int32 scaleFactorSrc= 1;
      Uint32 shiftFactorUVhorzSrc=0;
      Uint32 shiftFactorUVvertSrc=0;
    
      ipRunObj= &ipRun->ipRunObj;
      
      if (arg== NULL) {
         arg= &defArg;
         arg->multiCoreMode= ipRun->multiCoreMode;
         arg->alignImgBufWidth= 1;
      }
         
      numHorzBlocks= base->roiSize.width / base->procBlockSize.width;
      numVertBlocks= base->roiSize.height / base->procBlockSize.height;
      
      ipRun->multiCoreMode= arg->multiCoreMode;
      
      if ((numHorzBlocks * numVertBlocks)<= 2){
         
         // This will disable the scheduling in IP_run
         ipRun->singleBlockProcessing= 1;
         
         if ((numHorzBlocks * numVertBlocks)== 1) {
            ipRun->multiCoreMode= CPIS_MCORE_MODE_SINGLE;
            ipRunObj->numHorzBlocks= 1;
            ipRunObj->numVertBlocks= 1;
            }
         else {
            ipRun->multiCoreMode= CPIS_MCORE_MODE_DUAL_CLONE;
            
            if (numVertBlocks== 2)
               ipRun->dmaBlockTferType= CPIS_DMATFER_COL_WISE;
            else
               ipRun->dmaBlockTferType= CPIS_DMATFER_ROW_WISE;
               
            ipRunObj->numHorzBlocks= 2;
            ipRunObj->numVertBlocks= 1; 
            }
      }
      else {
         if (ipRun->dmaBlockTferType== CPIS_DMATFER_AUTO) {
            if ((ipRun->dmaBlockTferType=_CPIS_getBestDmaTferType(ipRun, numHorzBlocks, numVertBlocks))== -1)
            return -1;
         }
      
         if (ipRun->dmaBlockTferType== CPIS_DMATFER_ROW_WISE) {
            ipRunObj->numHorzBlocks= numHorzBlocks;
            ipRunObj->numVertBlocks= numVertBlocks;
         } else {
            ipRunObj->numVertBlocks= numHorzBlocks;
            ipRunObj->numHorzBlocks= numVertBlocks;
         }
      }
      
      trueSrcFormat= base->srcFormat[0] & ~CPIS_ALPHA;
      alphaOn= base->srcFormat[0] & CPIS_ALPHA;
    
      /* Calculate scaleFactor used to rescale the input widths */
      if ((trueSrcFormat) <= CPIS_BAYER_P){ /* if format is planar */
       
       if (alphaOn)
        ipRunObj->numDmaIn= 4;
       else 
        ipRunObj->numDmaIn= 3;
    
        switch (trueSrcFormat){
          case CPIS_YUV_420P:
            shiftFactorUVhorzSrc= shiftFactorUVvertSrc= 1;
          break;
          case CPIS_YUV_422P:
            shiftFactorUVhorzSrc= 1;
          break;
          case CPIS_YUV_411P:
            shiftFactorUVhorzSrc= 2;
          break;
        } /* switch */
        
      }/* if */
      else {
         
        if (trueSrcFormat== CPIS_YUV_420SP) {
         
         shiftFactorUVvertSrc= 1;
         if (alphaOn)
             ipRunObj->numDmaIn= 3;
         else
             ipRunObj->numDmaIn= 2;
             
        } else {
           if (alphaOn)
             ipRunObj->numDmaIn= 2;
           else
             ipRunObj->numDmaIn= 1;
           }
    
        scaleFactorSrc= _CPIS_sizeof(base->srcFormat[0]);
        
      }/* else */
    
      ipRunObj->numDmaIn= ipRunObj->numDmaIn*base->numInput;
    
      if (ipRunObj->numDmaIn > CPIS_MAX_SRC_CHANNELS) {
         CPIS_errno= CPIS_NOT_ENOUGH_EDMACHAN_ERROR;
         return -1;
      }
      
      /*ipRunObj->numDmaOut= 1; */
      /*ipRunObj->numDmaIn= 1; */
      /*
       *
       * Initialize dma parameters
       *
       */
      ipRunObj->dmaIn= &CPIS_obj.dmaIn[0];
      
      /* IP_RUN will do dynamic channel allocation through dmac module. */
      ipRunObj->dmaIn[0].dmaChNo = DMAC_CHAN_ANY;\
      /* We are going to initialize the dma transfer parameters normally */
      /* in which each block is separated from the previous one by a fixed offset. */
      /* so no need of transfer param table. */
      ipRunObj->dmaIn[0].useTferParamTable= 0;
      
      if (arg->alignImgBufWidth)
         roundBlockWidth= _CPIS_alignWithSIMD(base->procBlockSize.width);
      else
         roundBlockWidth= base->procBlockSize.width;
      
      ipRunObj->dmaIn[0].ddrAddr= (Uint32)base->srcBuf[0].ptr;
      ipRunObj->dmaIn[0].imgBufAddr= (Int32)(ipRun->imgbufInOfst + IMGBUF_A_BASE);
      
      if (ipRun->dmaBlockTferType== CPIS_DMATFER_ROW_WISE) {
         ddrOfstNextBlock= base->procBlockSize.width;
         ddrOfstNextBlockRow= base->srcBuf[0].stride * base->procBlockSize.height;
      }
      else {
         ddrOfstNextBlock= base->procBlockSize.height*base->srcBuf[0].stride;
         ddrOfstNextBlockRow= base->procBlockSize.width;
      }
      
      if (scaleFactorSrc > 0) { /* For any positif scaleFactorSrc, the scaleFactorSrc is a multiplier */
         ipRunObj->dmaIn[0].ddrWidth = scaleFactorSrc*base->srcBuf[0].stride;
         ipRunObj->dmaIn[0].imgBufWidth = scaleFactorSrc*roundBlockWidth;
         ipRunObj->dmaIn[0].blockWidth  = scaleFactorSrc*base->procBlockSize.width;
         ipRunObj->dmaIn[0].ddrOfstNextBlock= scaleFactorSrc*ddrOfstNextBlock;
         ipRunObj->dmaIn[0].ddrOfstNextBlockRow= scaleFactorSrc*ddrOfstNextBlockRow;
      }
      else { /* otherwise it is a divisor in order to handle type such as CPIS_1BIT */
         scaleFactorSrc= -scaleFactorSrc;
         ipRunObj->dmaIn[0].ddrWidth = base->srcBuf[0].stride/scaleFactorSrc;
         ipRunObj->dmaIn[0].imgBufWidth = roundBlockWidth/scaleFactorSrc;
         ipRunObj->dmaIn[0].blockWidth  = base->procBlockSize.width/scaleFactorSrc;
         ipRunObj->dmaIn[0].ddrOfstNextBlock= ddrOfstNextBlock/scaleFactorSrc;
         ipRunObj->dmaIn[0].ddrOfstNextBlockRow= ddrOfstNextBlockRow/scaleFactorSrc;
      }
        
      ipRunObj->dmaIn[0].blockHeight = base->procBlockSize.height;
      
      ipRun->imgbufLen= ipRunObj->dmaIn[0].imgBufWidth*ipRunObj->dmaIn[0].blockHeight; 
      oldScaleFactor= scaleFactorSrc;
    
      
      for (dmaIdx=1; dmaIdx<ipRunObj->numDmaIn; dmaIdx++) {
        
        if (alphaOn && (trueSrcFormat > CPIS_BAYER_P)) {
          if (trueSrcFormat!= CPIS_YUV_420SP && dmaIdx==1)
            scaleFactorSrc= 1;
          else
            if (trueSrcFormat== CPIS_YUV_420SP && dmaIdx==2) {
               scaleFactorSrc= 1;
               shiftFactorUVhorzSrc= 0;
               shiftFactorUVvertSrc= 0;
            }
            else
               scaleFactorSrc= 1;
        } 
        else if (trueSrcFormat == CPIS_YUV_420SP) /* if 420 semi-planar */
          scaleFactorSrc= 1;
        else if (trueSrcFormat >= CPIS_YUV_422IBE) /* if not planar */
          scaleFactorSrc= _CPIS_sizeof(base->srcFormat[dmaIdx]);
        else /* if planar */
          scaleFactorSrc= oldScaleFactor; 
    
        ipRunObj->dmaIn[dmaIdx].ddrAddr= (Uint32)base->srcBuf[dmaIdx].ptr;
        ipRunObj->dmaIn[dmaIdx].imgBufAddr= ipRunObj->dmaIn[0].imgBufAddr \
                                      + ipRun->imgbufLen;
        
        ipRunObj->dmaIn[dmaIdx].blockHeight = base->procBlockSize.height >> shiftFactorUVvertSrc;
                                      
        if (scaleFactorSrc > 0) { /* For any positif scaleFactorSrc, the scaleFactorSrc is a multiplier */
         ipRunObj->dmaIn[dmaIdx].ddrWidth = scaleFactorSrc*base->srcBuf[dmaIdx].stride;
         ipRunObj->dmaIn[dmaIdx].imgBufWidth = (scaleFactorSrc*roundBlockWidth) >> shiftFactorUVhorzSrc;
         ipRunObj->dmaIn[dmaIdx].blockWidth = (scaleFactorSrc*base->procBlockSize.width) >> shiftFactorUVhorzSrc;
         if (ipRun->dmaBlockTferType== CPIS_DMATFER_ROW_WISE) {
            ipRunObj->dmaIn[dmaIdx].ddrOfstNextBlock= (scaleFactorSrc*base->procBlockSize.width) >> shiftFactorUVhorzSrc;
            ipRunObj->dmaIn[dmaIdx].ddrOfstNextBlockRow= ipRunObj->dmaIn[dmaIdx].ddrWidth * ipRunObj->dmaIn[dmaIdx].blockHeight;
         }
         else {
            ipRunObj->dmaIn[dmaIdx].ddrOfstNextBlock= ipRunObj->dmaIn[dmaIdx].ddrWidth *ipRunObj->dmaIn[dmaIdx].blockHeight;
            ipRunObj->dmaIn[dmaIdx].ddrOfstNextBlockRow= (scaleFactorSrc*base->procBlockSize.width) >> shiftFactorUVhorzSrc;
         }    
        }
        else { /* otherwise it is a divisor in order to handle type such as CPIS_1BIT */
         scaleFactorSrc= -scaleFactorSrc;
         ipRunObj->dmaIn[dmaIdx].ddrWidth = base->srcBuf[dmaIdx].stride/scaleFactorSrc;
         ipRunObj->dmaIn[dmaIdx].imgBufWidth = (roundBlockWidth/scaleFactorSrc) >> shiftFactorUVhorzSrc;
         ipRunObj->dmaIn[dmaIdx].blockWidth  = (base->procBlockSize.width/scaleFactorSrc) >> shiftFactorUVhorzSrc;
         if (ipRun->dmaBlockTferType== CPIS_DMATFER_ROW_WISE) {
            ipRunObj->dmaIn[dmaIdx].ddrOfstNextBlock= (base->procBlockSize.width/scaleFactorSrc) >> shiftFactorUVhorzSrc;
            ipRunObj->dmaIn[dmaIdx].ddrOfstNextBlockRow= ipRunObj->dmaIn[dmaIdx].ddrWidth * ipRunObj->dmaIn[dmaIdx].blockHeight; 
            }
         else {
            ipRunObj->dmaIn[dmaIdx].ddrOfstNextBlock= ipRunObj->dmaIn[dmaIdx].ddrWidth * ipRunObj->dmaIn[dmaIdx].blockHeight;
            ipRunObj->dmaIn[dmaIdx].ddrOfstNextBlockRow= (base->procBlockSize.width/scaleFactorSrc) >> shiftFactorUVhorzSrc; 
         }
        }
        
        ipRun->imgbufLen+= ipRunObj->dmaIn[dmaIdx].imgBufWidth*ipRunObj->dmaIn[dmaIdx].blockHeight; 
    #ifdef _BENCHMARK_VICP
      ipRunObj->dmaIn[dmaIdx].blockWidth  = 16;
      ipRunObj->dmaIn[dmaIdx].blockHeight  = 1;
    #endif
        }
    #ifdef _BENCHMARK_VICP
      ipRunObj->dmaIn[0].blockWidth  = 16;
      ipRunObj->dmaIn[0].blockHeight  = 1;
    #endif
      return 0;
    }
    
    
    
    Int32 _CPIS_setDmaOutTransfers(CPIS_IpRun *ipRun, CPIS_BaseParms *base, CPIS_Arg *arg){
    
      /* This Dma structures are used to pass information about dma transfers to IP_RUN library */
      Int32 dmaIdx;
      IP_run *ipRunObj;
      Uint16 trueDstFormat, alphaOn;
      Int32 oldScaleFactor;
      Uint16 roundBlockWidth;
      Uint32 ddrOfstNextBlock, ddrOfstNextBlockRow;
      CPIS_Arg defArg;
      
      Int32 scaleFactorDst= 1;
      Uint32 shiftFactorUVhorzDst=0;
      Uint32 shiftFactorUVvertDst=0;
    
      ipRunObj= &ipRun->ipRunObj;
      
      if (arg== NULL) {
         arg= &defArg;
         arg->multiCoreMode= ipRun->multiCoreMode;
         arg->alignImgBufWidth= 1;
      }
      
      trueDstFormat= base->dstFormat[0] & ~CPIS_ALPHA;
      alphaOn= base->dstFormat[0] & CPIS_ALPHA;
    
      /* Calculate scaleFactor used to rescale the output widths */
      if (trueDstFormat<= CPIS_BAYER_P){ /* if format is planar */
       
       if (alphaOn)
        ipRunObj->numDmaOut= 4;
       else 
        ipRunObj->numDmaOut= 3;
       
       switch (trueDstFormat){
          case CPIS_YUV_420P:
            shiftFactorUVhorzDst= shiftFactorUVvertDst= 1;
            break;
          case CPIS_YUV_422P:
            shiftFactorUVhorzDst= 1;
            break;
          case CPIS_YUV_411P:
            shiftFactorUVhorzDst= 2;
            break;
        } /* switch */
        
      }/* if */
      else {
        if (trueDstFormat== CPIS_YUV_420SP) {
         shiftFactorUVvertDst= 1;
         if (alphaOn)
             ipRunObj->numDmaOut= 3;
         else
             ipRunObj->numDmaOut= 2;
             
        } else {
           if (alphaOn)
             ipRunObj->numDmaOut= 2;
           else
             ipRunObj->numDmaOut= 1;
           }
           
        scaleFactorDst= _CPIS_sizeof(base->dstFormat[0]);
        
        }/* else */
    
    
      /*
       *
       * Initialize dma parameters
       *
       */
       
      if (ipRun->dmaBlockTferType== CPIS_DMATFER_AUTO)
         ipRun->dmaBlockTferType= CPIS_DMATFER_ROW_WISE;
      
      ipRunObj->numDmaOut= ipRunObj->numDmaOut*base->numOutput;
      
      if (ipRunObj->numDmaOut > CPIS_MAX_DST_CHANNELS || (ipRunObj->numDmaIn + ipRunObj->numDmaOut > CPIS_obj.maxNumDma) ) {
          printf("Embedded Vision Framework error ! Number of DMA channels required by this function is %d and exceeds maximum allowed of %d\n", ipRunObj->numDmaIn + ipRunObj->numDmaOut, CPIS_obj.maxNumDma);
          CPIS_errno= CPIS_NOT_ENOUGH_EDMACHAN_ERROR;
         return -1;
      }
      
      ipRunObj->dmaOut= &CPIS_obj.dmaOut[0];
    
      /* IP_RUN will do dynamic channel allocation through dmac module. */
      ipRunObj->dmaOut[0].dmaChNo = DMAC_CHAN_ANY;
      /* We are going to initialize the dma transfer parameters normally */
      /* in which each block is separated from the previous one by a fixed offset. */
      /* so no need of transfer param table. */
      ipRunObj->dmaOut[0].useTferParamTable= 0;
    
      if (arg->alignImgBufWidth)
         roundBlockWidth= _CPIS_alignWithSIMD(base->procBlockSize.width);
      else
         roundBlockWidth= base->procBlockSize.width;
      
      if (ipRun->dmaBlockTferType== CPIS_DMATFER_ROW_WISE) {
         ddrOfstNextBlock= base->procBlockSize.width;
         ddrOfstNextBlockRow= base->dstBuf[0].stride * base->procBlockSize.height;
      }
      else {
         ddrOfstNextBlock= base->procBlockSize.height*base->dstBuf[0].stride;
         ddrOfstNextBlockRow= base->procBlockSize.width;
      }
      
      ipRunObj->dmaOut[0].ddrAddr= (Uint32)base->dstBuf[0].ptr;
      ipRunObj->dmaOut[0].imgBufAddr= (Int32)(ipRun->imgbufOutOfst[0] + IMGBUF_A_BASE);
      
      if (scaleFactorDst > 0) { /* For any positif scaleFactorDst, the scaleFactorDst is a multiplier */
         ipRunObj->dmaOut[0].ddrWidth = scaleFactorDst*base->dstBuf[0].stride;
         ipRunObj->dmaOut[0].imgBufWidth = scaleFactorDst*roundBlockWidth;
         ipRunObj->dmaOut[0].blockWidth  = scaleFactorDst*base->procBlockSize.width;
         ipRunObj->dmaOut[0].ddrOfstNextBlock= scaleFactorDst*ddrOfstNextBlock;
         ipRunObj->dmaOut[0].ddrOfstNextBlockRow= scaleFactorDst*ddrOfstNextBlockRow;
      }
      else { /* otherwise it is a divisor in order to handle type such as CPIS_1BIT */
         scaleFactorDst= -scaleFactorDst;
         ipRunObj->dmaOut[0].ddrWidth = base->dstBuf[0].stride/scaleFactorDst;
         ipRunObj->dmaOut[0].imgBufWidth = roundBlockWidth/scaleFactorDst;
         ipRunObj->dmaOut[0].blockWidth  = base->procBlockSize.width/scaleFactorDst;
         ipRunObj->dmaOut[0].ddrOfstNextBlock= base->procBlockSize.width/scaleFactorDst;
         ipRunObj->dmaOut[0].ddrOfstNextBlockRow= ddrOfstNextBlockRow/scaleFactorDst;
      }
      
      ipRunObj->dmaOut[0].blockHeight = base->procBlockSize.height;
      
      oldScaleFactor= scaleFactorDst;
      for (dmaIdx=1; dmaIdx<ipRunObj->numDmaOut; dmaIdx++) {
      
         if (alphaOn && (trueDstFormat > CPIS_BAYER_P)) {
             if (trueDstFormat!= CPIS_YUV_420SP && dmaIdx==1)
               scaleFactorDst= 1;
             else
               if (trueDstFormat== CPIS_YUV_420SP && dmaIdx==2) {
                  scaleFactorDst= 1;
                  shiftFactorUVhorzDst= 0;
                  shiftFactorUVvertDst= 0;
               }
               else
                  scaleFactorDst= 1;
        } 
        else if (trueDstFormat == CPIS_YUV_420SP) /* if 420 semi-planar */
          scaleFactorDst= 1;
        else if (trueDstFormat >= CPIS_YUV_422IBE) /* if not planar */
          scaleFactorDst= _CPIS_sizeof(base->dstFormat[dmaIdx]);
        else
          scaleFactorDst= oldScaleFactor;
      
        ipRunObj->dmaOut[dmaIdx].ddrAddr= (Uint32)base->dstBuf[dmaIdx].ptr;
        ipRunObj->dmaOut[dmaIdx].imgBufAddr= (Int32)(ipRun->imgbufOutOfst[dmaIdx] + IMGBUF_A_BASE);
        
        ipRunObj->dmaOut[dmaIdx].blockHeight = base->procBlockSize.height >> shiftFactorUVvertDst;
        
        if (scaleFactorDst > 0) { /* For any positif scaleFactorDst, the scaleFactorDst is a multiplier */
         ipRunObj->dmaOut[dmaIdx].ddrWidth = scaleFactorDst*base->dstBuf[dmaIdx].stride;
         ipRunObj->dmaOut[dmaIdx].imgBufWidth = (scaleFactorDst*roundBlockWidth) >> shiftFactorUVhorzDst;
         ipRunObj->dmaOut[dmaIdx].blockWidth  = (scaleFactorDst*base->procBlockSize.width) >> shiftFactorUVhorzDst;
         if (ipRun->dmaBlockTferType== CPIS_DMATFER_ROW_WISE) {
            ipRunObj->dmaOut[dmaIdx].ddrOfstNextBlock= (scaleFactorDst*base->procBlockSize.width) >> shiftFactorUVhorzDst;
            ipRunObj->dmaOut[dmaIdx].ddrOfstNextBlockRow= ipRunObj->dmaOut[dmaIdx].ddrWidth * ipRunObj->dmaOut[dmaIdx].blockHeight;
         }
         else {
            ipRunObj->dmaOut[dmaIdx].ddrOfstNextBlock= ipRunObj->dmaOut[dmaIdx].ddrWidth * ipRunObj->dmaOut[dmaIdx].blockHeight;
            ipRunObj->dmaOut[dmaIdx].ddrOfstNextBlockRow= (scaleFactorDst*base->procBlockSize.width) >> shiftFactorUVhorzDst;
         }  
        }
        else { /* otherwise it is a divisor in order to handle type such as CPIS_1BIT */
         scaleFactorDst= -scaleFactorDst;
         ipRunObj->dmaOut[dmaIdx].ddrWidth = base->dstBuf[dmaIdx].stride/scaleFactorDst;
         ipRunObj->dmaOut[dmaIdx].imgBufWidth = (roundBlockWidth/scaleFactorDst) >> shiftFactorUVhorzDst;
         ipRunObj->dmaOut[dmaIdx].blockWidth  = (base->procBlockSize.width/scaleFactorDst) >> shiftFactorUVhorzDst;
         if (ipRun->dmaBlockTferType== CPIS_DMATFER_ROW_WISE) {
            ipRunObj->dmaOut[dmaIdx].ddrOfstNextBlock= (base->procBlockSize.width/scaleFactorDst) >> shiftFactorUVhorzDst;
            ipRunObj->dmaOut[dmaIdx].ddrOfstNextBlockRow= ipRunObj->dmaOut[dmaIdx].ddrWidth * ipRunObj->dmaOut[dmaIdx].blockHeight; 
            }
         else {
            ipRunObj->dmaOut[dmaIdx].ddrOfstNextBlock= ipRunObj->dmaOut[dmaIdx].ddrWidth * ipRunObj->dmaOut[dmaIdx].blockHeight;
            ipRunObj->dmaOut[dmaIdx].ddrOfstNextBlockRow= (base->procBlockSize.width/scaleFactorDst) >> shiftFactorUVhorzDst; 
         }
        }
    #ifdef _BENCHMARK_VICP
      ipRunObj->dmaOut[dmaIdx].blockWidth  = 16;
      ipRunObj->dmaOut[dmaIdx].blockHeight  = 1;
    #endif
      }
    
    #ifdef _BENCHMARK_VICP
      ipRunObj->dmaOut[0].blockWidth  = 16;
      ipRunObj->dmaOut[0].blockHeight  = 1;
    #endif
      return 0;
    }
    
    
    Int32 _CPIS_setFirst(CPIS_IpRun *ipRun){
      
      if (CPIS_obj.numProcFunc== CPIS_obj.maxNumProcFunc){
        CPIS_errno= CPIS_MAXNUMFUNCREACHED;
        return -1;
      }
    
      _CPIS_setDemoMode(0);
      
    #if 0 /* enable this for later future vsersion */
      ipRun->imgbufOfst= CPIS_obj.imgbufOfst;
      ipRun->coefOfst= CPIS_obj.coefOfst;
      ipRun->coef1Ofst= CPIS_obj.coef1Ofst;
      ipRun->cmdOfst= CPIS_obj.cmdOfst;
      ipRun->cmd1Ofst= CPIS_obj.cmd1Ofst;
    #else
      ipRun->imgbufInOfst= 0;
      ipRun->imgbufOutOfst[0]= 0;
      ipRun->coefOfst= 0;
      ipRun->cmdOfst= 0;
      ipRun->coef1Ofst= 0;
      ipRun->cmd1Ofst= 0;
    #endif
    #ifdef _DUAL_CORE
      ipRun->multiCoreMode= CPIS_MCORE_MODE_MAXNUM_CLONE;//CPIS_MCORE_MODE_SINGLE;//CPIS_MCORE_MODE_MAXNUM_CLONE;
    #else
      ipRun->multiCoreMode= CPIS_MCORE_MODE_SINGLE;
    #endif
      ipRun->dmaBlockTferType= CPIS_DMATFER_AUTO;
      
      ipRun->context.action= CPIS_CONTEXT_NONE;
      ipRun->context.cmd0Ptr= NULL;
      ipRun->context.cmd1Ptr= NULL;
      ipRun->context.coef0Ptr= NULL;
      ipRun->context.coef1Ptr= NULL;
      ipRun->singleBlockProcessing= 0;
      
      ipRun->resetFlag= 0;
      ipRun->ipRunObj.cmdptr_ofst= ipRun->cmdOfst>>1;
      ipRun->ipRunObj.extension= NULL; /* NULL for DM350 */
      ipRun->ipRunObj.customExtension= NULL;
      
      _CPIS_switchBuffersToCPU();
    
      return 0;
    
    }
    
    Int32 _CPIS_setLast(CPIS_IpRun *ipRun, CPIS_ExecType execType){
      
    #if defined(_4MACS)
      IP_RUN_extension extension;
    #endif
      
      _CPIS_switchBuffersToCPU();
      
    #ifdef _SIMCOP
      if (ipRun->imgbufLen > 2*IMGBUF_SIZE_BYTES || ipRun->coefLen > COEFFBUF_SIZE_BYTES || ipRun->cmdLen > CMDBUF_SIZE_BYTES) {
    #else
      if (ipRun->imgbufLen > IMGBUF_SIZE_BYTES || ipRun->coefLen > COEFFBUF_SIZE_BYTES || ipRun->cmdLen > CMDBUF_SIZE_BYTES) {
    #endif
          CPIS_errno= CPIS_OUTOFMEM;
          printf("Out of mem, img buf= %d, coef = %d, cmd= %d\n", ipRun->imgbufLen, ipRun->coefLen, ipRun->cmdLen);
          return -1;
          };
    
      CPIS_obj.imgbufOfst=  ipRun->imgbufInOfst + ipRun->imgbufLen;
      CPIS_obj.coefOfst= ipRun->coefOfst + ipRun->coefLen;
      CPIS_obj.cmdOfst= ipRun->cmdOfst + ipRun->cmdLen;
      CPIS_obj.coef1Ofst= ipRun->coef1Ofst + ipRun->coef1Len;
      CPIS_obj.cmd1Ofst= ipRun->cmd1Ofst + ipRun->cmd1Len;
    
      ipRun->ipRunObj.cmdptr_ofst= ipRun->cmdOfst>>1;
      ipRun->ipRunObj.compCode= 0;
      
    #ifdef _BENCHMARK_EDMA
      *((Uint16*)CMDBUF_BASE + ipRun->ipRunObj.cmdptr_ofst)= 0x8000;
      *((Uint16*)CMD1BUF_BASE + (ipRun->cmd1Len>>1))= 0x8000;
    #endif
    
      if (CPIS_obj.waitCB)
        ipRun->ipRunObj.compIntEna= 1;
    #if defined(_4MACS)
      extension.magicWord= 0x12344321;
      
      extension.async= execType;
      
      if (ipRun->singleBlockProcessing== 1)
         extension.async|= 0x8000;
            
      ipRun->ipRunObj.extension= &extension;
      
      if ((ipRun->multiCoreMode & (~0x8000))== CPIS_MCORE_MODE_MAXNUM_CLONE){
         
        if (ipRun->context.action & CPIS_CONTEXT_RESTORE_CMD0) {
            ipRun->context.action |= CPIS_CONTEXT_RESTORE_CMD1;
            ipRun->context.cmd1Ptr= ipRun->context.cmd0Ptr;
            ipRun->cmd1Len= ipRun->cmdLen; 
        }
        
        if (ipRun->context.action & CPIS_CONTEXT_RESTORE_COEF0) {
            ipRun->context.action |= CPIS_CONTEXT_RESTORE_COEF1;
            ipRun->context.coef1Ptr= ipRun->context.coef0Ptr;
            ipRun->coef1Len= ipRun->coefLen;
        }
        
        if (_CPIS_multiCoreCloneDmaSetup(ipRun, 2)== -1) {
            _CPIS_printf("Reversing to single core processing.");
            ipRun->multiCoreMode= CPIS_MCORE_MODE_SINGLE;
            ipRun->context.action &= ~(CPIS_CONTEXT_SAVE_CMD1 | CPIS_CONTEXT_RESTORE_CMD1);
            CPIS_obj.cmd1Ofst= ipRun->cmd1Ofst + ipRun->cmd1Len;
         }
         else {
            _CPIS_multiCoreCloneMemSetup(ipRun, 2);
            extension.cmd1ptr_ofst= ipRun->cmdOfst>>1;
            ipRun->cmd1Ofst= ipRun->cmdOfst;
            ipRun->coef1Ofst= ipRun->coefOfst;
            }
      }
      else if ((ipRun->multiCoreMode & (~0x8000))== CPIS_MCORE_MODE_MAXNUM_SPLIT){
            if (ipRun->ipRunObj.numHorzBlocks <=3) {
               _CPIS_printf("Fatal error: Dual-core split mode cannot be enabled because number of horizontal block <=3");
               ipRun->multiCoreMode= CPIS_MCORE_MODE_SINGLE;
            }
            extension.cmd1ptr_ofst= ipRun->cmd1Ofst>>1;
            CACHE_writeBack(COEFF1BUF_BASE + ipRun->coef1Ofst, ipRun->coef1Len, 0);
            CACHE_writeBack(CMD1BUF_BASE + ipRun->cmd1Ofst, ipRun->cmd1Len, 1);
      }
      
      extension.iMXid= ipRun->multiCoreMode;
      
      extension.context= ipRun->context;
      extension.context.cmd0Len= ipRun->cmdLen;
      extension.context.cmd1Len= ipRun->cmd1Len;
      extension.context.coef0Len= ipRun->coefLen;
      extension.context.coef0Ofst= ipRun->coefOfst;
      extension.context.coef1Len= ipRun->coef1Len;
      extension.context.coef1Ofst= ipRun->coef1Ofst;
      
    #else
      ipRun->ipRunObj.extension= NULL;
    #endif
      ipRun->ipRunObj.customExtension= NULL;
      
      CACHE_writeBack(COEFFBUF_BASE + ipRun->coefOfst, ipRun->coefLen, 0);
      CACHE_writeBack(CMDBUF_BASE + ipRun->cmdOfst, ipRun->cmdLen, 1);
    
      if (IP_RUN_registerAlgo(&ipRun->ipRunObj, 0)== -1) {
         CPIS_errno= CPIS_ALGO_REGISTRATION_ERROR;
         return -1;
      }
      else
         CPIS_obj.numProcFunc++;
      
      /* In demo mode, we want to leave the other half unprocessed so we put a sleep */
      if (_CPIS_demoMode== 1) {
         IMGBUF_switch(SELCMD1BUF, CMD1BUFCPU);
         *((Uint16*)CMD1BUF_BASE)= 0x8000;
         IMGBUF_switch(SELCMD1BUF, CMD1BUFVICP);
      }
         
      return 0;
    
    }
    
    
    Int32 _CPIS_delete(CPIS_Handle handle){
      CPIS_IpRun *ipRunObj= (CPIS_IpRun *)handle;
      
      CPIS_obj.imgbufOfst-=  ipRunObj->imgbufLen;
      CPIS_obj.coefOfst-= ipRunObj->coefLen;
      CPIS_obj.cmdOfst-= ipRunObj->cmdLen;
      CPIS_obj.coef1Ofst-= ipRunObj->coef1Len;
      CPIS_obj.cmd1Ofst-= ipRunObj->cmd1Len;
      CPIS_obj.numProcFunc--;
      CPIS_obj.unlock(CPIS_obj.unlockArg);
       
      return 0;
    }
    
    /* Return number of bytes of the CPIS_Format */
    Int16 _CPIS_sizeof(CPIS_Format format){
    
        Uint16 trueFormat, alphaOn;
    
        trueFormat= format & ~CPIS_ALPHA;
        alphaOn= format & CPIS_ALPHA;
    
        if (alphaOn && trueFormat== CPIS_RGB_888)
            return 4;
        else
            return (_CPIS2VICP_sizeOfFormat[trueFormat]);
    
    }
    
    /* Return the corresponding VICP macro symbol for the CPIS_Format */
    Uint16 _CPIS_translateInputFormat(CPIS_Format format){
    
     return(_CPIS2VICP_inputFormat[format - CPIS_8BIT]);
     
    }
    
    /* Return the corresponding VICP macro symbol for the CPIS_Format */
    Uint16 _CPIS_translateOutputFormat(CPIS_Format format){
    
     return(_CPIS2VICP_outputFormat[format - CPIS_8BIT]);
     
    }
    
    /* This function validate the processing block dimensions
    against some predefined criteria and returns 0 if valid
    or -1 if not valid
    */
    Int32 _CPIS_isBlockDimValid(CPIS_BaseParms *base, Uint16 divisor, Uint16 maxNumPixels) {
    
      /* At this point none of the block dimensions should be 0. If yes then something
      has gone wrong ... */
      if (base->procBlockSize.width== 0 || base->procBlockSize.height== 0) {
         return -1;
      }
          
      /* procBlockSize.width must be multiple of divisor 
         it must divide the frame width
      */
      if (base->procBlockSize.width & (divisor-1) || (base->roiSize.width % (base->procBlockSize.width) )) {
         return -1;
      }  
      
      /* procBlockSize.height must divide the frame height */
      if (base->roiSize.height % base->procBlockSize.height) {
         return -1;
      }
    
      if (base->procBlockSize.width * base->procBlockSize.height > maxNumPixels){
         return -1;
      }
      
    return 0;
    }
    
    Int32 _CPIS_getFilterCascadeBlockDim(Uint16 numFilters, Uint16 outputBlockWidth, Uint16 outputBlockHeight, Uint16 *filterWidth, Uint16 *filterHeight,  Uint16 *inBlockWidth, Uint16 *inBlockHeight) {
    
        Int16 i;
    
        inBlockWidth[numFilters-1]= _CPIS_alignWithSIMD(outputBlockWidth + filterWidth[numFilters-1]-1);
        inBlockHeight[numFilters-1]= outputBlockHeight + filterHeight[numFilters-1]-1;
    
        for(i=numFilters-2;i>=0;i--){
            inBlockWidth[i]= _CPIS_alignWithSIMD(inBlockWidth[i+1] + filterWidth[i]-1);
            inBlockHeight[i]= inBlockHeight[i+1] + filterHeight[i]-1;
        }
    
        return 0;
    }
    
    Int32 _CPIS_getFilterCascadeBlockDim2(Uint16 numFilters, Uint16 outputBlockWidth, Uint16 outputBlockHeight, Uint16 *filterWidth, Uint16 *filterHeight,  Uint16 *inBlockWidth, Uint16 *inBlockHeight, Uint8 *dsW, Uint8 *dsH) {
    
        Int16 i;
    
        inBlockWidth[numFilters-1]= (outputBlockWidth<<dsW[numFilters-1]) + filterWidth[numFilters-1]-1;
        inBlockHeight[numFilters-1]= (outputBlockHeight<<dsH[numFilters-1]) + filterHeight[numFilters-1]-1;
    
        for(i=numFilters-2;i>=0;i--){
            inBlockWidth[i]= (inBlockWidth[i+1]<<dsW[i]) + filterWidth[i]-1;
            inBlockHeight[i]= (inBlockHeight[i+1]<<dsH[i]) + filterHeight[i]-1;
        }
    
        return 0;
    }
    /* ======================================================================== */
    /*                       End of file                                        */
    /* ------------------------------------------------------------------------ */
    /*            Copyright (c) 2008 Texas Instruments, Incorporated.           */
    /*                           All Rights Reserved.                           */
    /* ======================================================================== */
    
    
    

     

    regards,

     

    Victor