Other Parts Discussed in Thread: DRA821
Tool/software:
Hi DRA821 Managers,
I have some questions regarding the internal MCUs of the DRA821.
As you know, the DRA821 includes both the MCU island and the eMCU.
-
When using Suspend to RAM mode, could you provide details on the boot time for each of the MCUs and the Main domain upon wake-up?
-
Could you provide guidance on how the firmware for each MCU is initially downloaded and later updated?
For instance:-
Should the firmware be provided in a specific format, such as
.bin
? -
Is it possible to perform updates via the Main domain, using an internal bus to access the MCUs?
-
-
I assume an RTOS is required when using the MCUs.
Beyond FreeRTOS, are there Safety-certified OS options available that satisfy Cybersecurity and Functional Safety requirements? -
Is there any mode where the MCU island remains powered on and operational while the system is in Suspend to RAM?
-
In MCU-only mode and Suspend to RAM mode, could you describe the sequence of operations that occurs when the system enters Sleep and is later woken up by a wake-up source?
I would appreciate it if you could check and clarify these points.
Thank you, as always, for your continued support.
Best regards