Hi everyone,
When I start DM368-IPNC,always see the information follows from serial,and stops forever.it seems that the DM368 dead.But the voltage of DM368 is 3.3V at the same time.
U-Boot 1.3.4 (Nov 20 2011 - 08:57:19) DM368-IPNC-1.0.1
I2C: ready
DRAM: 128 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Bad block table found at page 65472, version 0x01
Bad block table found at page 65408, version 0x01
nand_bbt: ECC error while reading bad block table
128 MiB
In: serial
Out: serial
Err: serial
ARM Clock :- 432MHz
DDR Clock :- 340MHz
Ethernet PHY: GENERIC @ 0x01
Hit any key to stop autoboot: 4
Can anyone help me? Thanks!