This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO: Locatation of Launch config properties -> Common tab in CCS Theia 20.2.0

Part Number: CCSTUDIO


Tool/software:

Hi team,

Where can we find these "Common" options in CCS Theia 20.2.0 (Windows 10)?

BR,

Rudy

Screenshot from CCS 12.8

  • Hello,

    Where can we find these "Common" options in CCS Theia 20.2.0 (Windows 10)?

    This is functionality from the stock Eclipse IDE framework that earlier CCS version were based on. When CCS moved to the new Theia based IDE framework, this functionality was lost in the migration. It is something that others have requested and something we have discussed supporting in the future.

    Thanks

    ki

  • Update: There is no specific plan for everything in the "common" tab since much of it was Eclipse specific.

    However I noted that you highlighted the "output file" section. I assume you are interested in streaming the build logs to a file. This is on the roadmap:

    https://sir.ext.ti.com/jira/browse/EXT_EP-12245

    Thanks

    ki