Hi,
I am using OMAPL138 evm board . We wanted to use linux with that.. am using linuxsdk v 4_02_00_06.
Added 48 character lcd support in the kernel following the step given in
http://processors.wiki.ti.com/index.php/GSG:_Building_Software_Components_for_OMAP-L1#Character_LCD
Got three modules lcd.ko, backlight.ko and genericbl.ko
is that straight forward to insert these modules in to the kernel or any work is there?
What is the major and minor number for /dev/lcd if we are inserting these modules into filesystem built separately.
--
Zaheer