Other Parts Discussed in Thread: AM3517
Hello, I have a few questions about the AM3517
1. Do you know if anyone is using the AM3517 to operate large LCD displays on the order of >20” diagonal?
2. If yes to #1, are they connecting it directly to the 24-bit parallel digital output pins or are they using a VGA or DVI converter?
3. Does TI have any pre-built driver files to support various display types or sizes when driving them directly from the parallel interface?
4. Please provide any examples of customers using the AM3517 to operate large LCD displays.
Thanks!
Todd