This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64EVM: Feedback on https://dev.ti.com/tirex/content/tirex-product-tree/processors-devtools/am64x_gpevm_quick_start_guide.html

Part Number: TMDS64EVM
Other Parts Discussed in Thread: AM6442, SK-AM64B

Tool/software:

A few questions on the TMDS64EVM quick start guide AM64x EVM Quick Start Guide

1) Is this meant to encompass both the GP as well as the (B rev silicon) EVM?  You probably don't want to highlight all of the differences between a GP (rev A silicon) and the present rev B silicon (since Oct 2023) -- most everyone going forward should be on the rev B silicon AM6442

2) It is quite hard to order 16GB microSD cards nowadays (although the EVM ships with a Sandisk 16GB microSD card) - 64MB microSD cards are more plentiful in 2025. (Just be careful if you are trying to format that bigger microSD on a Win 11 PC as "FAT16" is not easy to specify in most user accessible Windows tools) 

Next feedback on the picture

3) On the left hand side = only need one of the 2 micro-USBs connected -- what is the reference designator? Should call out J26 (UART) as opposed to J28 (JTAG) in order that the MCU+ & CCS using folks do not get confused.

4) Also on the left hand side, you really should label SW1 as the "EVM power switch" . Note too that if you have J26 connected to the Linux PC prior to toggling SW1, some green LEDs may be on.

5) On the right hand side - RJ45's

    I would think it would be better to use the CPSW jack J14, aka eth0, instead of the dual stack J21(A&B) - unless the example is written to use the dual stack - comments?

    If you use the dual stack J21(A&B), after a good e2e discussion I had with Pekka (see (+) PROCESSOR-SDK-AM64X: Linux Academy (SDK v 10.1) - Wired Networking (1) no mention of eth2 (2) use ip instead of deprcated ifconfig? (3) reason for eth1 not showing up - Processors forum - Processors - TI E2E support forums  ) we need to ensure that the lower of the dual RJ45 stack (aka eth2) is used by default "out of the box" - the upper (aka eth1) one is disabled "out of the box".

6) Dealing with Writing the WIC image to an SD card, I know from past e2e's with Bin Lu, that maybe balenaEtcher had problems (I have only used that on Windows PCs) - I wonder if some reference to the  1.1.2. Create SD Card — Processor SDK AM64X Documentation section 1.1.2.3. Create SD Card using bmap-tools could be hyperlinked for Linux PC users here?

regards

Jim