This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: Unable to reboot

Part Number: TDA4VM-Q1


Tool/software:

Our development board's eMMC version fails to reboot (It keeps stopping at [ 33.447135] reboot: Restarting system. log provided below), but the NAND Flash version reboots normally. How should we troubleshoot and resolve this issue? Or what additional information should we provide?

log: root@j7-evm:~# reboot
[  OK  ] Stopped target RPC Port Mapper.
[  OK  ] Stopped target Timers.
[  OK  ] Stopped Daily rotation of log files.
[  OK  ] Stopped Daily Cleanup of Temporary Directories.
[  OK  ] Closed Load/Save RF Kill Switch Status /dev/r
                                                               Stopping TEE Supplicant...
[  OK  ] Stopped target System Time Synchronized.
[  OK  ] Stopped target System Time Set.[   26.785119] port 1 speed config is 1000

[   31.941854] R0: wlan: [731:E :SAP] Failed to find assoc ind list
         Stopping Starting udhcp of  wlan0...
[  OK  ] Stopped Job spooling tools.
[  OK  ] Stopped Periodic Command Scheduler.
[  OK  ] Stopped D-Bus System Message Bus.
[  OK  ] Stopped irqbalance daemon.
[  OK  ] Stopped Telephony service.
[  OK  ] Stopped TEE Supplicant.
[  OK  ] Stopped Wireless network connectivity (wlan0).
[  OK  ] Stopped Wait for Network to be Configured.
[  OK  ] Stopped Avahi mDNS/DNS-SD Stack.
[  OK  ] Stopped NFS status monitor for NFSv2/3 locking..
[  OK  ] Stopped Simple Network Man…ement Protocol (SNMP) Daemon..
[  OK  ] Stopped Starting udhcp of  wlan0.
[  OK  ] Stopped Getty on tty1.
[  OK  ] Stopped Serial Getty on ttyS2.
[  OK  ] Stopped Serial Getty on ttyS3.
[  OK  ] Stopped tda4_start.service.
[  OK  ] Stopped Reboot and dump vmcore via kexec.
[  OK  ] Stopped Load/Save Random Seed.
[  OK  ] Removed slice system-getty.slice.
[  OK  ] Removed slice system-serial\x2dgetty.slice.
[  OK  ] Stopped target Host and Network Name Lookups.
         Stopping Permit User Sessions...
         Stopping telnetd.service...
[  OK  ] Stopped Permit User Sessions.
[  OK  ] Stopped telnetd.service.
[  OK  ] Stopped target Network.
         Stopping Network Service...
         Stopping weston.service...
[  OK  ] Stopped weston.service.
[  OK  ] Stopped target Remote File Systems.
         Stopping rc.pvr.service...
[  OK  ] Stopped Update weston ini …ge based on the platform name.
[  OK  ] Stopped Network Service.
[  OK  ] Stopped target Network (Pre).
[  OK  ] Stopped IPv6 Packet Filtering Framework.
[  OK  ] Stopped IPv4 Packet Filtering Framework.
[  OK  ] Stopped rc.pvr.service.
[  OK  ] Stopped target Basic System.
[  OK  ] Stopped target Paths.
[  OK  ] Stopped Dispatch Password …ts to Console Directory Watch.
[  OK  ] Stopped Forward Password R…uests to Wall Directory Watch.
[  OK  ] Stopped target Slices.
[  OK  ] Removed slice User and Session Slice.
[  OK  ] Stopped target Sockets.
[  OK  ] Closed Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Closed D-Bus System Message Bus Socket.
[  OK  ] Closed Docker Socket for the API.
[  OK  ] Closed dropbear.socket.
[  OK  ] Stopped target System Initialization.
         Stopping Hardware RNG Entropy Gatherer Daemon...
[  OK  ] Stopped Apply Kernel Variables.
[  OK  ] Stopped Load Kernel Modules.
         Stopping Update UTMP about System Boot/Shutdown...
[  OK  ] Stopped Hardware RNG Entropy Gatherer Daemon.
[  OK  ] Stopped Update UTMP about System Boot/Shutdown.
[  OK  ] Stopped Create Volatile Files and Directories.
[  OK  ] Stopped target Local File Systems.
         Unmounting /media/ram...
         Unmounting /run/media/mmcblk0p1...
         Unmounting Temporary Directory (/tmp)...
         Unmounting /var/volatile...
[  OK  ] Unmounted /media/ram.
[  OK  ] Unmounted /run/media/mmcblk0p1.
[FAILED] Failed unmounting Temporary Directory (/tmp).
[  OK  ] Unmounted /var/volatile.
[  OK  ] Stopped target Swap.
[  OK  ] Reached target Unmount All Filesystems.
[  OK  ] Stopped File System Check on /dev/mmcblk0p1.
[  OK  ] Removed slice system-systemd\x2dfsck.slice.
[  OK  ] Stopped target Local File Systems (Pre).
[  OK  ] Stopped Remount Root and Kernel File Systems.
[  OK  ] Stopped Create Static Device Nodes in /dev.
[  OK  ] Reached target Shutdown.
[  OK  ] Reached target Final Step.
[  OK  ] Started Reboot.
[  OK  ] Reached target Reboot.
[   33.026119] port 2 linked with speed 1000
[   33.239137] systemd-shutdown[1]: Syncing filesystems and block devices.
[   33.252625] systemd-shutdown[1]: Sending SIGTERM to remaining processes...
[   33.269354] systemd-journald[190]: Received SIGTERM from PID 1 (systemd-shutdow).
[   33.304639] systemd-shutdown[1]: Sending SIGKILL to remaining processes...
[   33.317418] systemd-shutdown[1]: Unmounting file systems.
[   33.324170] [1114]: Unmounting '/tmp'.
[   33.329210] [1115]: Remounting '/' read-only in with options '(null)'.
[   33.344146] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[   33.358182] systemd-shutdown[1]: All filesystems unmounted.
[   33.363798] systemd-shutdown[1]: Deactivating swaps.
[   33.368810] systemd-shutdown[1]: All swaps deactivated.
[   33.374030] systemd-shutdown[1]: Detaching loop devices.
[   33.380839] systemd-shutdown[1]: All loop devices detached.
[   33.386410] systemd-shutdown[1]: Detaching DM devices.
[   33.391652] systemd-shutdown[1]: All DM devices detached.
[   33.397044] systemd-shutdown[1]: All filesystems, swaps, loop devices and DM devices detached.
[   33.411448] systemd-shutdown[1]: Syncing filesystems and block devices.
[   33.418203] systemd-shutdown[1]: Rebooting.
[   33.447135] reboot: Restarting system