Hello,
I would like to use a single SPI port on C6748 to connect to multiple DACs using SPI0 multiple Chip Selects. I would also like to use EDMA channels to transfer the data from memory buffer to a specific SPI connected DAC, then move to the next DAC, and the next. Is this possible? Can EDMA channel be tied to a specific SPI Chip Select?
Thank you,
Alex