Part Number: AM6422
Tool/software:
Hello,
We are developing using SDK 8.6, implementing Ethernet-based Telnet functionality on R5F under FreeRTOS. Currently, there's an issue: during implementation, when the Ethernet connection is successfully established, the system uses the printf function to send data over Ethernet. How can this printf be mapped to the Ethernet interface? Additionally, when the Ethernet connection is disconnected, printf should revert to printing via the serial port.
Is such functionality achievable?Is it feasible to directly use printf as previously implemented on other platforms in the current environment?