This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 serial boot mode

Now i have switch to uart boot mode ,and My board is dm368 ,when download program is prompts :

 

Waiting for DONE...

DONE received.  Sending the UBL...

 100% [                                                              ]

                              UBL sent....

DONE received.  UBL was accepted.

UBL transmitted successfully.

Waiting for SFT on the DM36x...

        Target: Starting UART Boot...

        Target: BOOTUBL

BOOTUBL commmand received. Returning CMD and command...
CMD value sent.  Waiting for DONE...
        Target:    DONE
DONE received. Command was accepted.
Command not recognized!
It prompt "commnad not recognized!" !