Hi htere,
I'm writing TCP3E driver of TMS320C6670. I encountered some questions and hope you could help me.
I'm using queue 704 as a TX queue and 708 as a RX queue. And I wanna use Accumulator high priority channel 0 to monitor these two queues. How do I configure the
PDSP? The threshhold of queue 704 is 4 and that of queue 708 is 1. How does channel 0 identify each queue's interrupt? Is there some example projects on the issue I
encounted?
Now, the situation is queue 704 interrupt can be responsed, but queue 708 ISR cann't be serviced. Need some help.
Thank you
Best regards
Nick