This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 EVM board ping response slowly.



Hi, we found a strange thing in Davinci EVM board.

if we ping the board with 32 bytes or 24000 bytes data, everything is OK.

But if we ping it with 4000 bytes, the time is changed randomly.

the following is the printing:

ping 192.168.2.199 -t -l 4000

Pinging 192.168.2.199 with 4000 bytes of data:

Reply from 192.168.2.199: bytes=4000 time=878ms TTL=64

Reply from 192.168.2.199: bytes=4000 time=887ms TTL=64

Reply from 192.168.2.199: bytes=4000 time=886ms TTL=64

Reply from 192.168.2.199: bytes=4000 time=885ms TTL=64

Reply from 192.168.2.199: bytes=4000 time=692ms TTL=64

Reply from 192.168.2.199: bytes=4000 time=1ms TTL=64

Reply from 192.168.2.199: bytes=4000 time=882ms TTL=64


I checked with my friends. They are using DM365 in their products. All have the same problem.

This would cause serious delay in video data transferring.

We are using  kernel  Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.0.0

Any suggestion?

Thanks very much