Tool/software:
Hi TI experts,
I know the TI EVM is using main_uart0 as debug console. But we plan use main_uart1 (B24 / C24) as the debug console
So I would like to ask the following questions:
1. Is it possible to switch the debug console to main_uart1?
2. If so, what are the required changes in the device tree and bootloader configuration?
3. Is there any dependency or limitation with using main_uart1 for this purpose?