Part Number: CCSTUDIO
Other Parts Discussed in Thread: MATHLIB
Tool/software:
I am currently using CCS installed on a Linux OS, but I am unable to detect mathlib.c674x using the following command line.eclipse -nosplash -application com.ti.common.core.initialize -rtsc.productDiscoveryPath <mathlib install path>
In my environment, I'm unable to use the GUI, so it is necessary to perform the detection via command line.
Could you please advise me on how to detect mathlib.c674x using command line commands?
The CCS and mathlib.c674x versions are as follows:
- CCS: 12.8.1
- mathlib_c674x: 3.1.2.1