Other Parts Discussed in Thread: DM3730
Hi All,
Our platform is based on DM3730 processor. we are using Windows CE 6.0 BSP supporting EVMDM3730.
we are not able to set GPIO126, GPIO129 and GPIO163. but the pins were tested under CCS code.
here is the following code used for setting the pins GPIO126 and GPIO129
----------------------
OMAP_GPIO_REGS* pGpio;
DWORD GpioNumber;
OMAP_SYSC_PADCONFS_WKUP_REGS *g_pSyscPadWkupRegs = OALPAtoUA(OMAP_SYSC_PADCONFS_WKUP_REGS_PA);
OMAP_SYSC_GENERAL_REGS* pSyscGeneralRegs = OALPAtoUA(OMAP_SYSC_GENERAL_REGS_PA);
OMAP_SYSC_GENERAL_WKUP_REGS_DM3730 *GenWkpRegs = OALPAtoUA(OMAP_SYSC_GENERAL_WKUP_REGS_DM3730_PA);
SETREG32(&pSyscGeneralRegs->CONTROL_PBIAS_LITE, (PBIASLITEVMODE0|PBIASLITEPWRDNZ0|PBIASLITEVMODE1|PBIASLITEPWRDNZ1));
SETREG32(&GenWkpRegs->CONTROL_WKUP_CTRL, (0x40));
OUTREG16(&g_pSyscPadWkupRegs->CONTROL_PADCONF_GPIO126, (INPUT_DISABLE | PULL_INACTIVE | MUX_MODE_4));
OUTREG16(&g_pSyscPadWkupRegs->CONTROL_PADCONF_GPIO129, (INPUT_DISABLE | PULL_INACTIVE | MUX_MODE_4));
GpioNumber = 126;
pGpio = OALPAtoUA(OMAP_GPIO4_REGS_PA);
GpioNumber -= 96;
CLRREG32(&pGpio->OE, 1 << GpioNumber);
SETREG32(&pGpio->DATAOUT, 1 << GpioNumber);
GpioNumber = 129;
pGpio = OALPAtoUA(OMAP_GPIO5_REGS_PA);
GpioNumber -= 128;
CLRREG32(&pGpio->OE, 1 << GpioNumber);
SETREG32(&pGpio->DATAOUT, 1 << GpioNumber);
-----------------------------------------------------------------------------------------
please guide us.
regards,