This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem of Using Tuning Tool output on the target platform

Part Number: PROCESSOR-SDK-J721S2


Tool/software:

Hello,

We are in the process of tuning the ISP (SDK 09_01_00_22) for my own sensor.

Using the app_single_cam software, we can capture RAW images and YUV images, but there is an issue with white balance. Therefore, the following steps were taken:

  1. I followed the AWB Plugin Guide in DCC to perform white balance calibration for the camera and generated the mycamera_awb_alg_ti3_tuning.xml file. And put it in ti-processor-sdk-rtos-j721s2-evm-09_01_00_06/imaging/sensor_drv/src/mycamera/dcc_xmls

  2. Used generate_dcc.sh to generate the dcc_2a_mycamera.h file.

  3. Added my camera’s configuration in the app_iss_common.c file (in the functions appIssGetDCCSize2A and appIssGetDCCBuff2A), run make imaging_scrub & make vision_apps_scrub then make imaging&make vision_apps
    but the white balance is still not correct.

I printed out DCCSize2A, found that the size is the same as dcc_2a_imx390, not my expected value (25587)."sensor name : mycamera,size : 22321,sensor_wdr_mode:0. "

 

 dcc_buff_size_driver = appIssGetDCCSize2A(obj->sensor_name, sensor_wdr_mode);
 printf("sensor name : %s,size : %d,sensor_wdr_mode:%u\n",obj->sensor_name,dcc_buff_size_driver,sensor_wdr_mode);

Even after I forcibly modified both the size and buffer to match my own settings, the white balance is still incorrect.

//dcc_buff_size_driver = appIssGetDCCSize2A(obj->sensor_name, sensor_wdr_mode);
dcc_buff_size_driver = DCC_2A_mycamera_DCC_CFG_NUM_ELEM;
    
//status = appIssGetDCCBuff2A(obj->sensor_name, sensor_wdr_mode,  dcc_2a_buf, dcc_buff_size_driver);
memcpy(dcc_2a_buf, dcc_2a_mycamera_linear, dcc_buff_size_driver);

I saved RAW and YUV images under the following three conditions:

1.dcc_buff_size_driver = -1

2.dcc_buff_size_driver = appIssGetDCCSize2A(obj->sensor_name, sensor_wdr_mode);
status = appIssGetDCCBuff2A(obj->sensor_name, sensor_wdr_mode, dcc_2a_buf, dcc_buff_size_driver);  

3.dcc_buff_size_driver = DCC_2A_mycamera_DCC_CFG_NUM_ELEM;
memcpy(dcc_2a_buf, dcc_2a_mycamera_linear, dcc_buff_size_driver);  

RAW_YUV_IMG.zip

By the way, in the function appDccUpdatefromFS, is the break statement missing in the case blocks?

int32_t appDccUpdatefromFS(char* sensor_name, uint8_t wdr_mode,
                        vx_node node_viss, uint32_t viss_node_index,
                        vx_node node_aewb, uint32_t aewb_node_index,
                        vx_node node_ldc, uint32_t ldc_node_index,
                        vx_context context)
{
    char dcc_dir_path[MAX_FOLDER_NAME_LEN];
     char op_mode[8];
    int dcc_num_bytes;
    int dcc_bytes_read;
    uint8_t * dcc_buf;
    switch(wdr_mode)
    {
        case 0:
            /*Linear mode*/
            snprintf(op_mode, 8, "%s", "linear");
        default:
            /*WDR mode*/
            snprintf(op_mode, 8, "%s", "wdr");
    }