I would like to know more about the transfer controller in the EDMA3 controller.
Is it possible to use TC0 and TC1 at the same time without conflict?
I would like to be able to have two DMA transfers going on at the same time without interference.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to know more about the transfer controller in the EDMA3 controller.
Is it possible to use TC0 and TC1 at the same time without conflict?
I would like to be able to have two DMA transfers going on at the same time without interference.
Marko,
Please see the EDMA3 User's Guide to learn more about the EDMA3 controller. There is a lot to know, and we wrote the User's Guide to help you find the answers you need.
In the Training section of TI.com, there is a training video set for the C6474. This may not be the device you are particularly interested in, but the EDMA3 module is close to the same on every device that includes it. It may be helpful for you to review all of the modules. In particular, the EDMA3/QDMA/IDMA Module may help you understand some of the features and options available within the EDMA3 module. You can find the complete video set here.
Regards,
RandyP
If you need more help, please reply back. If this answers the question, please click Verify Answer , below.