Part Number: AM62P
Tool/software:
This FAQ describes how to enable BT.656 in embedded syncs mode for AM62P.
Similar patch can be created for other AM6x SoCs as well.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM62P
Tool/software:
This FAQ describes how to enable BT.656 in embedded syncs mode for AM62P.
Similar patch can be created for other AM6x SoCs as well.
Note: AM62P only supports BT.656 with embedded syncs, and not with discrete syncs.
Please apply the following patch series for BT.656 progressive mode (may need to apply manually on different SDK version):
AM62P_BT656_patch_series.zip
Please take a look at the following TRM section specifying which data lines are utilized in BT.656 mode.
Note: In progressive BT.656/BT.1120 mode the maximum output resolution will be limited, as it requires two pixel clock cycles to send out one pixel.
When facing issue in using above patch, please create E2E ticket with output logs of the following commands:
kmsprint #Note the connector ID from here modetest -M tidss -s <Connector ID>:720x480@NV12 -v rwmem 0x3020b000+0x200 modetest -M tidss
For hints on enabling BT.656 interlaced, refer to patches towards the end of the following thread (patches applicable on top of BT.656 progressive patches in above post):
RE: AM62A7-Q1: TIDSS: BT656 with interlaced mode