Hi, I'm working with OMAP L-138 EVM, C6748. DSP/BIOS 5x.
I'd like to configure GPIO interrupts in my application. The TMS320C674x Tech Reference Guide 19.2.10.1 Interrupt Events and Requests says :
"... The device supports interrupts from single GPIO signals, interrupts from banks of GPIO signals, or both..."
TMS320C674x Tech Reference Guide 19.2.10.2 Enabling GPIO Interrupt Events says:
"...GPIO interrupt events are enabled in banks of 16 by setting the appropriate bit(s) in the GPIO interrupt per-bank enable register (BINTEN)..."
TMS320C674x OMAP L1x GPIO Guide says the same.
Is it possible to configure each GPIO pin to generate interrupt separately or it is available only through the whole bank interrupt/event? If it is possible to make it, how I actually do that?
Thank, Anatoly.