This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to download my program to dm6437's flash?



I have try to download my program to dm6437's flash, but the program can not boot after reboot. I doubt the cmd file is not correct. Additional i want to know how to distinguish these two cases: load all the program to run in ram after boot, load part of the program to run in ram after boot. In different cases should we how to write the correct cmd file? The following is my cmd file.

-l rts64plus.lib
-l lib\SEED_DEC6437bsl.lib

-stack          0x01000000      /* Stack Size */
-heap           0x05000000      /* Heap Size */

MEMORY
{  
    BOOT_RAM:   o = 0x10800000  l = 0x00000400
    INT:        o = 0x10800400  l = 0x00000400        
    L2RAM:      o = 0x10800800  l = 0x00020000
    DDR2:       o = 0x80000000  l = 0x8000000
}

 

SECTIONS
{
    .boot_load  >   BOOT_RAM
    .bss        >   L2RAM
    .cinit      >   L2RAM
    .cio        >   L2RAM
    .const      >   L2RAM
    .data       >   L2RAM
    .far        >   L2RAM
    .stack      >   DDR2
    .switch     >   L2RAM
    .sysmem     >   DDR2
    .text       >   DDR2
 .vectors > INT
    .ddr2       >   DDR2

}