Other Parts Discussed in Thread: AM1808, OMAP-L138, DA8XX, PMP
We wish to flash a JFFS2 Linux root filesystem and kernel image into the 512MB NAND on the AM1808 EVM and then boot completely from NAND.
Steps are given below
- compiled uboot with nand support
- UBL and uboot for nand are flashed on NAND
- given boot arguments are:
setenv bootcmd 'nand read.e 0xc1180000 0x780000 0x4600000; nboot.e 0xc0700000 280000 0x220000; bootm 0xc0700000 '
setenv bootargs console=ttyS2,115200n8 rw ip=172.16.19.14 nfsroot=172.16.13.100:/home/filesys,nolock mem=32M
While booting, MTD partition for NAND is not created.
How to get MTD NAND partition?
Can someone please help me understand the recommended method for programming the NAND filesystem and kernel image?
The boot logs (nfs boot) are attched inline,
U-Boot > boot
nand - NAND sub-system
Usage:
nand info - show available NAND devices
nand device [dev] - show or set current device
nand read - addr off|partition size
nand write - addr off|partition size
read/write 'size' bytes starting at offset 'off'
to/from memory address 'addr', skipping bad blocks.
nand erase [clean] [off size] - erase 'size' bytes from
offset 'off' (entire device if not specified)
nand bad - show bad blocks
nand dump[.oob] off - dump page
nand scrub - really clean NAND erasing bad blocks (UNSAFE)
nand markbad off [...] - mark bad block(s) at offset (UNSAFE)
nand biterr off - make a bit error at offset (UNSAFE)
** Device 3145728 not available
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.33-rc4
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2189752 Bytes = 2.1 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.33-rc4 (bcg@BCGA100) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #5 PREEMPT Thu Dec 15 10:01:14 IST 2011
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DA850/OMAP-L138/AM18xx EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci da850/omap-l138 variant 0x0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: console=ttyS2,115200n8 rw ip=172.16.19.14 nfsroot=172.16.13.100:/home/bcg/work/sdk_1_10_00_00/filesys,nolock mem=32M
PID hash table entries: 128 (order: -3, 512 bytes)
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 27824KB available (4152K code, 317K data, 148K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 149.50 BogoMIPS (lpj=747520)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 144 gpio irqs
regulator: core version 0.5
NET: Registered protocol family 16
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
regulator: VDCDC1: 3200 <--> 3300 mV at 3300 mV
regulator: VDCDC2: 1750 <--> 3300 mV at 3300 mV
regulator: VDCDC3: 950 <--> 1375 mV at 1200 mV
regulator: LDO1: 1800 mV
regulator: LDO2: 1150 <--> 1300 mV at 1200 mV
DA850/OMAP-L138 EVM UI card detected
i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL)
Switching to clocksource timer0_1
musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0
Waiting for USB PHY clock good...
musb_hdrc: USB Host mode controller at fee00000 using DMA, IRQ 58
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
EMAC: MII PHY configured, RMII PHY will not be functional
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
JFS: nTxBlock = 217, nTxLock = 1739
msgmni has been set to 54
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found Sharp_LK043T1DG01 panel
Console: switching to colour frame buffer device 60x34
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A
console [ttyS2] enabled
brd: module loaded
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci
ata1: SATA max UDMA/133 irq 67
spi_davinci spi_davinci.1: DaVinci SPI driver in EDMA mode
Using RX channel = 18 , TX channel = 19 and event queue = 1
m25p80 spi1.0: m25p64 (8192 Kbytes)
Creating 4 MTD partitions on "m25p80":
0x000000000000-0x000000040000 : "U-Boot"
0x000000040000-0x000000050000 : "U-Boot Environment"
0x000000050000-0x0000007f0000 : "Linux"
0x0000007f0000-0x000000800000 : "MAC Address"
Read MAC addr from EEPROM: ff:ff:ff:ff:ff:ff
spi_davinci spi_davinci.1: Controller at 0xfef0e000
console [netcon0] enabled
netconsole: network logging started
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 2
ohci ohci.0: irq 59, io mem 0x01e25000
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
input: TPS6507x Touchscreen as /devices/platform/i2c-gpio.1/i2c-1/1-0048/input/input0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
omap_rtc: already running
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v0.1.0)
watchdog watchdog: heartbeat 60 sec
cpuidle: using governor ladder
cpuidle: using governor menu
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Advanced Linux Sound Architecture Driver Version 1.0.21.
usbcore: registered new interface driver snd-usb-audio
No device for DAI tlv320aic3x
asoc: tlv320aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DA850/OMAP-L138 EVM (tlv320aic3x)
TCP cubic registered
NET: Registered protocol family 17
Clocks: disable unused i2c1
Clocks: disable unused emac
Clocks: disable unused aemif
Clocks: disable unused spi0
Clocks: disable unused mcbsp0
Clocks: disable unused mcbsp1
Clocks: disable unused vpif
ata1: SATA link down (SStatus 0 SControl 300)
regulator_init_complete: incomplete constraints, leaving LDO2 on
regulator_init_complete: incomplete constraints, leaving LDO1 on
regulator_init_complete: incomplete constraints, leaving VDCDC3 on
regulator_init_complete: incomplete constraints, leaving VDCDC2 on
regulator_init_complete: incomplete constraints, leaving VDCDC1 on
davinci_emac_probe: using random MAC addr: 52:fb:db:89:d1:34
emac-mii: probed
omap_rtc omap_rtc: setting system clock to 2000-01-01 01:01:03 UTC (946688463)
eth0: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=1:00, id=7c0f1)
IP-Config: Guessing netmask 255.255.0.0
IP-Config: Complete:
device=eth0, addr=172.16.19.14, mask=255.255.0.0, gw=255.255.255.255,
host=172.16.19.14, domain=, nis-domain=(none),
bootserver=255.255.255.255, rootserver=172.16.13.100, rootpath=
Looking up port of RPC 100003/2 on 172.16.13.100
PHY: 1:00 - Link is Up - 100/Full
Looking up port of RPC 100005/1 on 172.16.13.100
VFS: Mounted root (nfs filesystem) on device 0:13.
Freeing init memory: 148K
ipv6: disagrees about version of symbol module_layout
INIT: Entering runlevel: 5
Starting telnet daemon.
Starting syslogd/klogd: ipv6: disagrees about version of symbol module_layout
done
Starting thttpdipv6: disagrees about version of symbol module_layout
.
ipv6: disagrees about version of symbol module_layout
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org SDR ttyS2
Arago 2010.03 SDR ttyS2
SDR login: