This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: The first 8MB of eMMC is used as a boot-only area, and the area after 8MB is used as a user area, but is it possible to operate with files as with AM335x?

Expert 2680 points
Part Number: SK-AM62


Tool/software:

Hi All,

About eMMC
When setting First Boot SD / BackUp Boot eMVC
The first 8MB of eMMC is used as a boot-only area, and the area after 8MB is used as a user area, but is it possible to operate with files as with AM335x?
*3.2.2.16.8. Created partitions in eMMC UDA, but could not boot


SDD Layout
In the FAT area:
tiboot3.bin
tispl.bin
u-boot.img
uEnv.txt
Is ‘environment (128 KB)’ referring to uFnv.txt?

Best Regards,

Ito