Part Number: TDA4VM
Tool/software:
I am working with the app_multi_cam application from the Processor SDK RTOS 11.00 on the J721E EVM.
I have applied the multi_cam_file_input.patchand copied the multi_cam_file folder from multi_cam_file_test_data.zip to the following location on the EVM:
/opt/vision_apps/test_data/multi_cam_file/
I have a few clarifications regarding the configuration:
- Should I enable
test_mode = 1inside the config file, or should it be passed as a command-line argument?
./vx_app_multi_cam.out --cfg app_multi_cam_config.cfg --test - Do I need to mention the input file path (
/opt/vision_apps/test_data/multi_cam_file/) explicitly in the config file, or is it hardcoded in program? - Below is the config file I’m using. Can you please confirm if it’s correct for running file-based input?
# test mode: 1-enable # if this is enabled, fake data will be run into the sensor port test_mode 1 # sensor selection # 0 : IMX390 # 1 : AR0233 # 2 : AR0820 sensor_index 0 # LDC 0-disable, 1-enable enable_ldc 0 # Channel mask in decimal. Indicates number and positions of cameras selected. # For e.g. channel_mask = 15 (0x0F) indicates that first 4 cameras are enabled channel_mask 15 # Number of frames to run num_frames_to_run 1000000 # Show output in HDMI/eDP, 0-disable, 1-enable display_option 1 # Supported usecase options 0, 1 usecase_option 0 # enable interactive mode 0-noninteractive, 1-interactive is_interactive 1 # enable writing final output 0-disable, 1-enable en_out_img_write 1 # enable writing csix output 0-disable, 1-enable en_out_capture_write 0 # enable writing viss output 0-disable, 1-enable en_out_viss_write 0 # enable writing ldc output 0-disable, 1-enable en_out_ldc_write 0 # Number of frames to write per 's' command, num_frames_to_write 1 # Number of frames to skip per 's' command, Eg. 0-no frame skip, 1-skip 1 frame, 2-skip 2 frames etc. num_frames_to_skip 0 # path to write the processed frames output_file_path /opt/vision_apps/app_cam_out # Disable error detection by default enable_error_detection 0 # Configure HWA frequency in application enable_configure_hwa_freq 0 # Configures VPAC/DMPAC frequency # Valid values: 0 for VPAC 650 MHz, DMPAC 520 MHz; 1 for VPAC 720 MHz, DMPAC 480 MHz # Valid only if enable_configure_hwa_freq is set to 1 hwa_freq_config 0 # Flag to bypass split graph configuration bypass_split_graph 0