This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: Kernel panic on AM4376

Part Number: AM4376

Tool/software:

Posting on behalf of the customer.

We are performing certification testing with UL, during testing device suddenly stop working.

We check all the voltages, it was fine. After that We enabled the Linux Kernel Low level log in the Linux kernel configuration. After enabling this, we got the below kernel panic error. I think, this error is internal to the Processor bus.

omap_l3_noc 44000000.ocp: L3 application error: target 13 mod:1 (unclearable)
8<--- cut here -----
Unhandled fault: imprecise external abort (0x1406) at 0x75d7b3e5e5
pgd = (ptrval)l)
[75d7b3e5] *pgd=0000000000c
Internal error: : 1406 [#1] PREEMPT_RT ARMRM
Modules linked in:c
CPU: 0 PID: 1 Comm: swapper Tainted: G        W         5.10.100-rt62-g204ec708dc #6
Hardware name: Generic AM43 (Flattened Device Tree)
PC is at sysc_probe+0xd88/0x1554
LR is at sysc_probe+0xcd4/0x1554
pc : [<c04e88c8>]    lr : [<c04e8814>]    psr: a0000013
sp : c1469de8  ip : 00000000  fp : c0b35dfc
r10: 00000028  r9 : 00000000  r8 : c0b3627c
r7 : c1585c10  r6 : 00000000  r5 : c10e9f28  r4 : c1730540
r3 : 00000074  r2 : ffffffed  r1 : 00000074  r0 : 00000000
Flags: NzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment none
Control: 10c53c7d  Table: 80004059  DAC: 00000051
Process swapper (pid: 1, stack limit = 0x(ptrval))))
Stack: (0xc1469de8 to 0xc146a000)0)