Part Number: AM62A7
Other Parts Discussed in Thread: SK-AM62A-LP
Tool/software:
Hello.
I'm Jae Young Choi.
We are experiencing a boot issue on our custom board using the AM62A7 and would like to ask for your support.
Is it possible that the AM62A7 fails to boot when its internal temperature is high?
Experiment Setup:
- Custom board based on TI AM62A7
- Both A53 and C7x cores are used
- PROCESSOR-SDK-LINUX-AM62A 10.00.00.08
- Booting from eMMC
Observed Behavior:
- After operating for 2–3 hours, some boards fail to power up when turned off and on again.
- This occurs in about 2 to 3 out of 10 boards.
- The failure is not consistent: different boards may fail on different attempts.
- At the time of failure, the MPU temperature is around 80°C to 90°C.
Expected Behavior:
- The board should boot successfully even when the temperature is around 80°C to 90°C.
Additional Experiment:
- When heating the SoC area with a heat gun to raise the temperature above 90°C, the board consistently fails to power on.
However, if the power is turned off and left for about 5 minutes to cool down, all boards power on normally again.
Questions:
- Can high internal temperature at power-on prevent the AM62A7 from booting?
- The datasheet specifies a maximum operating temperature of 125°C, but is there a lower temperature limit specifically for the power-on or boot process?
Serial Log:
U-Boot SPL 2024.04-ti-g818c76aed67f (Nov 11 2024 - 15:14:15 +0900) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13568 bytes Trying to boot from MMC1
Thank you.
Best regards.