This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

M2-CC3351: Integrating in SK-AM62B-P1

Part Number: M2-CC3351
Other Parts Discussed in Thread: AM625

Tool/software:

Hi,

I brought the M2-CC3351 Bluetooth/Wi-Fi module, and I am only interested in using the Bluetooth module. I am confused about how to enable the Bluetooth via the device tree. I have attached the DTS file to this. 

I'm a bit confused with the register/pin number for this - SPI2_D0, SPID1, SPI2_clk, and SPI2_CSO, from my understanding, are RTs, CTs, TxD, and RxD. In the Excel sheet, they got a different AWL number for each. Can you help me find which are the exact pins and register to enable Bluetooth?
am62b.pdf8585.AM62X_pin_attributes_rev_B1.xls2318.k3-am625-sk.txt

  • Hello Fnu,

    Sorry for the delay; I was Out of office. 

    In order to use bluetooth, you must first enable the wifi driver. But first, let me understand, which SDK version are you intending to use on the AM62?

    If you are using the M2-CC3351, then there is no way to connect it to the Am62 with SPI as the M.2 will only uses SDIO.