This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Missing Firmware Files After Flashing Linux SDK – How to Generate and Deploy from RTOS SDK?

Part Number: TDA4VM

Tool/software:

Hello,

We have successfully flashed the prebuilt Linux SDK for J721E onto an SD card and booted the EVM. However, during boot we observed that the following firmware files are missing:

j7-main-r5f1_0-fw

j7-main-r5f1_1-fw

j7-mcu-r5f0_1-fw

These firmware files are part of the RTOS SDK, and are required for the remoteproc framework to boot the R5F cores.

We understand that we need to:

Build the corresponding .out files from the RTOS SDK.

Use tiobj2bin along with llvm-objcopy (from the TI CGT ARM LLVM toolchain) to convert .out to .bin.

Copy the .bin files to /lib/firmware/ on the EVM.

However, we found that llvm-objcopy is not present on our host system, and we haven't installed the TI ARM LLVM toolchain yet.


what is done so for
---------------------------
followed the official RTOS SDK build process (Linux + RTOS mode):

cd /u/new_sdk/RTOS
tar -xvf ti-processor-sdk-rtos-j721e-evm-11_00_00_06.tar.gz

cd ti-processor-sdk-rtos-j721e-evm-11_00_00_06
./sdk_builder/scripts/setup_psdk_rtos.sh

# Edited build flags for Linux+RTOS mode
vi sdk_builder/build_flags.mak

cd sdk_builder
make sdk -j$(nproc)

After the build completed, we got the .out firmware files in:
vision_apps/out/J721E/R5F/FREERTOS/release/


Questions:
--------------
What are the official steps to install the ti-cgt-armllvm toolchain on a Linux host?and please provides its link.

Once installed, how exactly do we use tiobj2bin with llvm-objcopy to generate the required .bin firmware?

Are there any specific versions of ti-cgt-armllvm that we must use with SDK 11.0.0?

U-Boot SPL 2025.01-00410-g70667128cb5b (Apr 04 2025 - 18:20:14 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.9--v11.00.09+ (Fancy Rat)')
Trying to boot from MMC2
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Loading Environment from nowhere... OK
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.12.0(release):11.00.09-dirty
NOTICE:  BL31: Built : 12:35:58, Mar 24 2025
I/TC: 
I/TC: OP-TEE version: 4.5.0-73-gef1ebdc23-dev (gcc version 13.3.0 (GCC)) #1 Tue Feb  4 11:33:18 UTC 2025 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
I/TC: SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.9--v11.00.09+ (Fancy Rat)')
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: HUK Initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2025.01-00410-g70667128cb5b-dirty (Apr 04 2025 - 18:20:14 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.9--v11.00.09+ (Fancy Rat)')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2
Skipping authentication on GP device
Skipping authentication on GP device


U-Boot 2025.01-00410-g70667128cb5b-dirty (Apr 04 2025 - 18:20:14 +0000)

SoC:   J721E SR1.0 GP
Model: Texas Instruments J721e EVM
Board: J721EX-PM2-SOM rev E7
DRAM:  2 GiB (total 4 GiB)
Core:  149 devices, 36 uclasses, devicetree: separate
Flash: 0 Bytes
MMC:   mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from nowhere... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net:   eth0: ethernet@46000000port@1
Hit any key to stop autoboot:  2  0 
=> setenv rproc_fw_binaries 
=> boot
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
907 bytes read in 2 ms (442.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
gpio: pin gpio@22_17 (gpio 281) value is 1
gpio: pin gpio@22_16 (gpio 280) value is 0
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
22256128 bytes read in 462 ms (45.9 MiB/s)
124702 bytes read in 7 ms (17 MiB/s)
Working FDT set to 88000000
1783 bytes read in 4 ms (434.6 KiB/s)
11521 bytes read in 5 ms (2.2 MiB/s)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
   Loading Device Tree to 000000008fede000, end 000000008fffffff ... OK
Working FDT set to 8fede000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[    0.000000] Linux version 6.12.17-ti-00773-gcdcaeac783e3-dirty (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Thu Apr  3 17:42:36 UTC 2025
[    0.000000] KASLR disabled due to lack of seed
[    0.000000] Machine model: Texas Instruments J721e EVM
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: legacy bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x00000008e0000000, size 512 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000008e0000000..0x00000008ffffffff (524288 KiB) map reusable linux,cma
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 624 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x0000000880000000..0x00000008a6ffffff (638976 KiB) nomap non-reusable vision-apps-core-heap-memory-hi@880000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000e4800000, size 24 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-buffers@e4800000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000e4800000..0x00000000e5ffffff (24576 KiB) nomap non-reusable vision-apps-r5f-virtual-eth-buffers@e4800000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000e4000000, size 8 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-queues@e4000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000e4000000..0x00000000e47fffff (8192 KiB) nomap non-reusable vision-apps-r5f-virtual-eth-queues@e4000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000d8000000, size 192 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@d8000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000d8000000..0x00000000e3ffffff (196608 KiB) nomap non-reusable vision-apps-core-heap-memory-lo@d8000000
[    0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
[    0.000000] OF: reserved mem: 0x00000000b8000000..0x00000000d7ffffff (524288 KiB) map non-reusable vision_apps_shared-memories
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000b2100000, size 95 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c71-memory@b2100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000b2100000..0x00000000b7ffffff (97280 KiB) nomap non-reusable vision-apps-c71-memory@b2100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000b2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@b2000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000b2000000..0x00000000b20fffff (1024 KiB) nomap non-reusable vision-apps-c71-dma-memory@b2000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 96 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@ac000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000ac000000..0x00000000b1ffffff (98304 KiB) nomap non-reusable vision-apps-dma-memory@ac000000
[    0.000000] OF: reserved mem: 0x00000000aa000000..0x00000000abffffff (32768 KiB) nomap non-reusable vision-apps-rtos-ipc-memory-region
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a9100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a9100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a9100000..0x00000000a9ffffff (15360 KiB) nomap non-reusable vision-apps-c66-memory@a9100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a9000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a9000000..0x00000000a90fffff (1024 KiB) nomap non-reusable vision-apps-c66-dma-memory@a9000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a8100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a8100000..0x00000000a8ffffff (15360 KiB) nomap non-reusable vision-apps-c66-memory@a8100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a8000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a8000000..0x00000000a80fffff (1024 KiB) nomap non-reusable vision-apps-c66-dma-memory@a8000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a7100000..0x00000000a7ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a7100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a7000000..0x00000000a70fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a7000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a6100000..0x00000000a6ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a6100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a6000000..0x00000000a60fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a6000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4100000..0x00000000a5ffffff (31744 KiB) nomap non-reusable vision-apps-r5f-memory@a4100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a40fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a4000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a3ffffff (31744 KiB) nomap non-reusable vision-apps-r5f-memory@a2100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a2000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a1100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a1000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0100000..0x00000000a0ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a0100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a00fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a0000000
[    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000008ffffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000b7ffffff]
[    0.000000]   node   0: [mem 0x00000000b8000000-0x00000000d7ffffff]
[    0.000000]   node   0: [mem 0x00000000d8000000-0x00000000e5ffffff]
[    0.000000]   node   0: [mem 0x00000000e6000000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000008a6ffffff]
[    0.000000]   node   0: [mem 0x00000008a7000000-0x00000008ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.5
[    0.000000] percpu: Embedded 22 pages/cpu s51672 r8192 d30248 u90112
[    0.000000] Detected PIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: Spectre-v3a
[    0.000000] CPU features: detected: Spectre-BHB
[    0.000000] CPU features: detected: ARM erratum 1742098
[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),1m(ospi.sysfw),256k(ospi.env.backup),57344k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs) root=PARTUUID=d1826cc2-02 rw rootfstype=ext4 rootwait
[    0.000000] Unknown kernel command line parameters "mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),1m(ospi.sysfw),256k(ospi.env.backup),57344k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs)", will be passed to user space.
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1048576
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 2.
[    0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: 	RCU event tracing is enabled.
[    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=512 to nr_cpu_ids=2.
[    0.000000] 	Trampoline variant of Tasks RCU enabled.
[    0.000000] 	Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=2.
[    0.000000] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=2.
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 960 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: GICD_CTRL.DS=0, SCR_EL3.FIQ=1
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8a7800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x00000008a7040000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008a7050000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008515] Console: colour dummy device 80x25
[    0.013083] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.023755] pid_max: default: 32768 minimum: 301
[    0.028516] LSM: initializing lsm=capability,selinux
[    0.033624] SELinux:  Initializing.
[    0.037482] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.045047] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.065338] rcu: Hierarchical SRCU implementation.
[    0.070248] rcu: 	Max phase no-delay instances is 1000.
[    0.075703] Timer migration: 1 hierarchy levels; 8 children per group; 1 crossnode level
[    0.084363] EFI services will not be available.
[    0.089112] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[    0.102342] Detected PIPT I-cache on CPU1
[    0.102392] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[    0.102405] GICv3: CPU1: using allocated LPI pending table @0x00000008a7060000
[    0.102434] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[    0.102516] smp: Brought up 1 node, 2 CPUs
[    0.131866] SMP: Total of 2 processors activated.
[    0.136671] CPU: All CPU(s) started at EL2
[    0.140869] CPU features: detected: 32-bit EL0 Support
[    0.146118] CPU features: detected: CRC32 instructions
[    0.151384] alternatives: applying system-wide alternatives
[    0.157332] Memory: 1687636K/4194304K available (12928K kernel code, 1254K rwdata, 4644K rodata, 2752K init, 639K bss, 1974408K reserved, 524288K cma-reserved)
[    0.172433] devtmpfs: initialized
[    0.183385] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.193362] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.206504] 27152 pages in range for non-PLT usage
[    0.206517] 518672 pages in range for PLT usage
[    0.211645] pinctrl core: initialized pinctrl subsystem
[    0.221858] DMI not present or invalid.
[    0.227058] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.233714] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[    0.241013] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.249010] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.257142] audit: initializing netlink subsys (disabled)
[    0.262853] audit: type=2000 audit(0.200:1): state=initialized audit_enabled=0 res=1
[    0.263078] thermal_sys: Registered thermal governor 'step_wise'
[    0.270777] thermal_sys: Registered thermal governor 'power_allocator'
[    0.276937] cpuidle: using governor menu
[    0.287709] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.294674] ASID allocator initialised with 65536 entries
[    0.305788] /bus@100000/interrupt-controller@1800000: Fixed dependency cycle(s) with /bus@100000/interrupt-controller@1800000
[    0.326544] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.333497] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.339902] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.346837] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.353240] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.360175] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.366577] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.373512] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.380994] k3-chipinfo 43000014.chipid: Family:J721E rev:SR1.0 JTAGID[0x0bb6402f] Detected
[    0.393563] iommu: Default domain type: Translated
[    0.398468] iommu: DMA domain TLB invalidation policy: strict mode
[    0.404959] SCSI subsystem initialized
[    0.408986] usbcore: registered new interface driver usbfs
[    0.414613] usbcore: registered new interface driver hub
[    0.420058] usbcore: registered new device driver usb
[    0.425525] pps_core: LinuxPPS API ver. 1 registered
[    0.430598] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.439936] PTP clock support registered
[    0.443959] EDAC MC: Ver: 3.0.0
[    0.447320] scmi_core: SCMI protocol bus registered
[    0.452457] FPGA manager framework
[    0.455969] Advanced Linux Sound Architecture Driver Initialized.
[    0.462620] vgaarb: loaded
[    0.465555] clocksource: Switched to clocksource arch_sys_counter
[    0.471927] VFS: Disk quotas dquot_6.6.0
[    0.475949] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.486725] Carveout Heap: Exported 512 MiB at 0x00000000b8000000
[    0.493022] NET: Registered PF_INET protocol family
[    0.498107] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.506501] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[    0.515256] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.523180] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.531327] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[    0.539232] TCP: Hash tables configured (established 16384 bind 16384)
[    0.545972] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.552855] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.560239] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.566303] RPC: Registered named UNIX socket transport module.
[    0.572361] RPC: Registered udp transport module.
[    0.577165] RPC: Registered tcp transport module.
[    0.581969] RPC: Registered tcp-with-tls transport module.
[    0.587573] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.594156] NET: Registered PF_XDP protocol family
[    0.599061] PCI: CLS 0 bytes, default 64
[    0.603721] Initialise system trusted keyrings
[    0.608388] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[    0.615144] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.621244] NFS: Registering the id_resolver key type
[    0.626424] Key type id_resolver registered
[    0.630698] Key type id_legacy registered
[    0.634801] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.641651] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.670999] Key type asymmetric registered
[    0.675188] Asymmetric key parser 'x509' registered
[    0.680198] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.687851] io scheduler mq-deadline registered
[    0.692485] io scheduler kyber registered
[    0.696597] io scheduler bfq registered
[    0.702798] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[    0.709221] pinctrl-single 11c000.pinctrl: 173 pins, size 692
[    0.715515] pinctrl-single 104200.pinctrl: 20 pins, size 80
[    0.721278] pinctrl-single 104280.pinctrl: 8 pins, size 32
[    0.727467] ledtrig-cpu: registered to indicate activity on CPUs
[    0.737160] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.745330] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00101faf)
[    0.753960] arm-smmu-v3 36600000.iommu: allocated 65536 entries for cmdq
[    0.761080] arm-smmu-v3 36600000.iommu: allocated 32768 entries for evtq
[    0.768236] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs
[    0.779637] loop: module loaded
[    0.783483] megasas: 07.727.03.00-rc1
[    0.789160] tun: Universal TUN/TAP device driver, 1.6
[    0.794947] VFIO - User Level meta-driver version: 0.3
[    0.800937] usbcore: registered new interface driver usb-storage
[    0.807452] i2c_dev: i2c /dev entries driver
[    0.812513] sdhci: Secure Digital Host Controller Interface driver
[    0.818843] sdhci: Copyright(c) Pierre Ossman
[    0.823427] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.829631] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.836623] usbcore: registered new interface driver usbhid
[    0.842327] usbhid: USB HID core driver
[    0.846872] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 (0,8000003f) counters available
[    0.856731] optee: probing for conduit method.
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[    0.861291] optee: revision 4.5 (ef1ebdc23034a804)
[    0.877761] optee: dynamic shared memory is enabled
[    0.888048] optee: initialized driver
[    0.888129] random: crng init done
[    0.893325] Initializing XFRM netlink socket
[    0.899675] NET: Registered PF_PACKET protocol family
[    0.904876] Key type dns_resolver registered
[    0.913070] registered taskstats version 1
[    0.917459] Loading compiled-in X.509 certificates
[    0.929359] ti-sci 44083000.system-controller: ABI: 4.0 (firmware rev 0x000b '11.0.9--v11.00.09+ (Fancy Rat)')
[    1.056646] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz
[    1.063155] pca953x 1-0020: supply vcc not found, using dummy regulator
[    1.069995] pca953x 1-0020: using no AI
[    1.090297] pca953x 1-0022: supply vcc not found, using dummy regulator
[    1.097115] pca953x 1-0022: using AI
[    1.101947] omap_i2c 2000000.i2c: bus 1 rev0.12 at 400 kHz
[    1.108140] pca953x 2-0020: supply vcc not found, using dummy regulator
[    1.114967] pca953x 2-0020: using no AI
[    1.134079] omap_i2c 2030000.i2c: bus 2 rev0.12 at 400 kHz
[    1.140057] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 137 domain created
[    1.148624] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 131 domain created
[    1.157976] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 213 domain created
[    1.166611] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[    1.181474] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[    1.191382] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[    1.198150] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[    1.207921] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211
[    1.218100] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[    1.224876] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[    1.233047] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 204, base_baud = 6000000) is a 8250
[    1.242769] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 205, base_baud = 3000000) is a 8250
[    1.251701] printk: legacy console [ttyS2] enabled
[    1.251701] printk: legacy console [ttyS2] enabled
[    1.261390] printk: legacy bootconsole [ns16550a0] disabled
[    1.261390] printk: legacy bootconsole [ns16550a0] disabled
[    1.274292] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 206, base_baud = 3000000) is a 8250
[    1.283557] 2840000.serial: ttyS0 at MMIO 0x2840000 (irq = 207, base_baud = 3000000) is a 8250
[    1.294109] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[    1.333563] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    1.343004] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    1.351279] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[    1.364140] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    1.371351] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64, Policers 8
[    1.378790] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:1
[    1.389445] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[    1.398488] mmc0: CQHCI version 5.10
[    1.437590] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[    1.522154] mmc0: Command Queue Engine enabled
[    1.526619] mmc0: new HS200 MMC card at address 0001
[    1.536017] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[    1.541500] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB
[    1.547145] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB
[    1.552624] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (239:0)
[    1.594131] tps6594-esm tps6594-esm.3.auto: error -ENODEV: ESM not supported for revision 1 PMIC
[    1.607184] tps6594-rtc tps6594-rtc.4.auto: registered as rtc0
[    1.769645] tps6594-esm tps6594-esm.9.auto: error -ENODEV: ESM not supported for revision 1 PMIC
[    1.782713] tps6594-rtc tps6594-rtc.10.auto: registered as rtc1
[    1.795292] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[    1.802794] j721e-pcie 2900000.pcie:       IO 0x0010001000..0x0010010fff -> 0x0010001000
[    1.810884] j721e-pcie 2900000.pcie:      MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[    1.818969] j721e-pcie 2900000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    2.933962] j721e-pcie 2900000.pcie: PCI host bridge to bus 0000:00
[    2.940247] pci_bus 0000:00: root bus resource [bus 00-ff]
[    2.945732] pci_bus 0000:00: root bus resource [io  0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[    2.955196] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[    2.962076] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400 PCIe Root Port
[    2.969372] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[    2.979019] pci 0000:00:00.0: PCI bridge to [bus 00]
[    2.983975] pci 0000:00:00.0:   bridge window [io  0x0000-0x0fff]
[    2.990057] pci 0000:00:00.0:   bridge window [mem 0x00000000-0x000fffff]
[    2.996834] pci 0000:00:00.0:   bridge window [mem 0x00000000-0x000fffff 64bit pref]
[    3.004635] pci 0000:00:00.0: supports D1
[    3.008635] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[    3.014383] pci 0000:00:00.0: VF BAR 0 [mem 0x00000000-0x003fffff 64bit]
[    3.021070] pci 0000:00:00.0: VF BAR 0 [mem 0x00000000-0x00ffffff 64bit]: contains BAR 0 for 4 VFs
[    3.032119] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    3.040252] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[    3.046870] pci 0000:00:00.0: VF BAR 0 [mem 0x10400000-0x113fffff 64bit]: assigned
[    3.054429] pci 0000:00:00.0: PCI bridge to [bus 01]
[    3.059387] pci_bus 0000:00: resource 4 [io  0x0000-0xffff]
[    3.064948] pci_bus 0000:00: resource 5 [mem 0x10011000-0x17ffffff]
[    3.071268] pcieport 0000:00:00.0: of_irq_parse_pci: failed with rc=-22
[    3.078048] pcieport 0000:00:00.0: PME: Signaling with IRQ 655
[    3.084060] pcieport 0000:00:00.0: AER: enabled with IRQ 655
[    3.090013] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[    3.097501] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
[    3.105584] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
[    3.113664] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    4.225811] j721e-pcie 2910000.pcie: PCI host bridge to bus 0001:00
[    4.232080] pci_bus 0001:00: root bus resource [bus 00-ff]
[    4.237557] pci_bus 0001:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[    4.247191] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[    4.254067] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400 PCIe Root Port
[    4.261363] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[    4.271007] pci 0001:00:00.0: PCI bridge to [bus 00]
[    4.275962] pci 0001:00:00.0:   bridge window [io  0x0000-0x0fff]
[    4.282043] pci 0001:00:00.0:   bridge window [mem 0x00000000-0x000fffff]
[    4.288821] pci 0001:00:00.0:   bridge window [mem 0x00000000-0x000fffff 64bit pref]
[    4.296603] pci 0001:00:00.0: supports D1
[    4.300604] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[    4.308397] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    4.316513] pci_bus 0001:01: busn_res: [bus 01-ff] end is updated to 01
[    4.323125] pci 0001:00:00.0: PCI bridge to [bus 01]
[    4.328083] pci_bus 0001:00: resource 4 [io  0x10000-0x1ffff]
[    4.333820] pci_bus 0001:00: resource 5 [mem 0x18011000-0x1fffffff]
[    4.340145] pcieport 0001:00:00.0: of_irq_parse_pci: failed with rc=-22
[    4.346913] pcieport 0001:00:00.0: PME: Signaling with IRQ 657
[    4.352913] pcieport 0001:00:00.0: AER: enabled with IRQ 657
[    4.358877] j721e-pcie 2920000.pcie: host bridge /bus@100000/pcie@2920000 ranges:
[    4.366362] j721e-pcie 2920000.pcie:       IO 0x4400001000..0x4400010fff -> 0x0000001000
[    4.374460] j721e-pcie 2920000.pcie:      MEM 0x4400011000..0x4407ffffff -> 0x0000011000
[    4.382553] j721e-pcie 2920000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    5.493677] j721e-pcie 2920000.pcie: PCI host bridge to bus 0002:00
[    5.499946] pci_bus 0002:00: root bus resource [bus 00-ff]
[    5.505422] pci_bus 0002:00: root bus resource [io  0x20000-0x2ffff] (bus address [0x1000-0x10fff])
[    5.514466] pci_bus 0002:00: root bus resource [mem 0x4400011000-0x4407ffffff] (bus address [0x00011000-0x07ffffff])
[    5.524987] pci 0002:00:00.0: [104c:b00d] type 01 class 0x060400 PCIe Root Port
[    5.532282] pci_bus 0002:00: 2-byte config write to 0002:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[    5.541927] pci 0002:00:00.0: PCI bridge to [bus 00]
[    5.546882] pci 0002:00:00.0:   bridge window [io  0x0000-0x0fff]
[    5.552964] pci 0002:00:00.0:   bridge window [mem 0x00000000-0x000fffff]
[    5.559744] pci 0002:00:00.0:   bridge window [mem 0x00000000-0x000fffff 64bit pref]
[    5.567521] pci 0002:00:00.0: supports D1
[    5.571522] pci 0002:00:00.0: PME# supported from D0 D1 D3hot
[    5.579325] pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    5.587433] pci_bus 0002:01: busn_res: [bus 01-ff] end is updated to 01
[    5.594047] pci 0002:00:00.0: PCI bridge to [bus 01]
[    5.599006] pci_bus 0002:00: resource 4 [io  0x20000-0x2ffff]
[    5.604745] pci_bus 0002:00: resource 5 [mem 0x4400011000-0x4407ffffff]
[    5.611408] pcieport 0002:00:00.0: of_irq_parse_pci: failed with rc=-22
[    5.618189] pcieport 0002:00:00.0: PME: Signaling with IRQ 659
[    5.624184] pcieport 0002:00:00.0: AER: enabled with IRQ 659
[    5.630761] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[    5.642063] ti-udma 31150000.dma-controller: Channels: 122 (tchan: 61, rchan: 61, gp-rflow: 16)
[    5.656571] 8 fixed-partitions partitions found on MTD device 47040000.spi.0
[    5.663666] Creating 8 MTD partitions on "47040000.spi.0":
[    5.669184] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    5.675322] 0x000000080000-0x000000280000 : "ospi.tispl"
[    5.681115] 0x000000280000-0x000000680000 : "ospi.u-boot"
[    5.686989] 0x000000680000-0x0000006a0000 : "ospi.env"
[    5.692671] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup"
[    5.698908] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[    5.704726] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[    5.710610] 0x000003fe0000-0x000004000000 : "ospi.phypattern"
[    5.716900] cadence-qspi 47040000.spi: Pattern not found. Skipping calibration.
[    5.727410] 8 fixed-partitions partitions found on MTD device 47050000.spi.0
[    5.734462] Creating 8 MTD partitions on "47050000.spi.0":
[    5.739936] 0x000000000000-0x000000080000 : "qspi.tiboot3"
[    5.746004] 0x000000080000-0x000000280000 : "qspi.tispl"
[    5.751809] 0x000000280000-0x000000680000 : "qspi.u-boot"
[    5.757722] 0x000000680000-0x0000006a0000 : "qspi.env"
[    5.763346] 0x0000006a0000-0x0000006c0000 : "qspi.env.backup"
[    5.769591] 0x0000006c0000-0x0000007c0000 : "qspi.sysfw"
[    5.775408] 0x000000800000-0x000003fc0000 : "qspi.rootfs"
[    5.781307] 0x000003fe0000-0x000004000000 : "qspi.phypattern"
[    5.788153] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[    5.829562] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    5.838977] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    5.847251] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[    5.860108] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    5.867318] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64, Policers 8
[    5.874726] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:1
[    5.894167] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[    5.906400] mmc1: CQHCI version 5.10
[    5.911176] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[    5.918260] clk: Disabling unused clocks
[    5.944586] PM: genpd: Disabling unused power domains
[    5.945578] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[    5.949782] ALSA device list:
[    5.960068]   No soundcards found.
[    5.963645] Waiting for root device PARTUUID=d1826cc2-02...
[    6.018227] mmc1: new ultra high speed DDR50 SDHC card at address aaaa
[    6.025093] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[    6.033812]  mmcblk1: p1 p2
[    6.558827] EXT4-fs (mmcblk1p2): recovery complete
[    6.564458] EXT4-fs (mmcblk1p2): mounted filesystem 0b4bc077-9173-4f02-9077-d360666c5df7 r/w with ordered data mode. Quota mode: none.
[    6.576569] VFS: Mounted root (ext4 filesystem) on device 179:98.
[    6.586430] devtmpfs: mounted
[    6.590590] Freeing unused kernel memory: 2752K
[    6.595196] Run /sbin/init as init process
[    6.907004] systemd[1]: System time before build time, advancing clock.
[    6.955540] NET: Registered PF_INET6 protocol family
[    6.961073] Segment Routing with IPv6
[    6.964754] In-situ OAM (IOAM) with IPv6
[    7.005892] systemd[1]: systemd 255.18^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified)
[    7.037765] systemd[1]: Detected architecture arm64.

Welcome to Arago 2025.01!

[    7.056991] systemd[1]: Hostname set to <j721e-evm>.
[    7.281724] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    7.383858] systemd[1]: Queued start job for default target Graphical Interface.
[    7.424619] systemd[1]: Created slice Slice /system/getty.
[  OK  ] Created slice Slice /system/getty.
[    7.442797] systemd[1]: Created slice Slice /system/modprobe.
[  OK  ] Created slice Slice /system/modprobe.
[    7.462745] systemd[1]: Created slice Slice /system/serial-getty.
[  OK  ] Created slice Slice /system/serial-getty.
[    7.482493] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    7.501800] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password Requests to Console Directory Watch.
[    7.521719] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password Requests to Wall Directory Watch.
[    7.541651] systemd[1]: Expecting device /dev/ttyS2...
         Expecting device /dev/ttyS2...
[    7.557678] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Path Units.
[    7.573624] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    7.589618] systemd[1]: Reached target Slice Units.
[  OK  ] Reached target Slice Units.
[    7.605628] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[    7.652253] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    7.669711] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    7.691100] systemd[1]: Listening on Process Core Dump Socket.
[  OK  ] Listening on Process Core Dump Socket.
[    7.709844] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    7.730239] systemd[1]: Listening on Journal Audit Socket.
[  OK  ] Listening on Journal Audit Socket.
[    7.745993] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    7.765987] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    7.782025] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    7.804681] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    7.821904] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    7.837937] systemd[1]: Listening on User Database Manager Socket.
[  OK  ] Listening on User Database Manager Socket.
[    7.881778] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    7.899806] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    7.921914] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    7.937937] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[    7.955619] systemd[1]: Mounting Temporary Directory /tmp...
         Mounting Temporary Directory /tmp...
[    7.974075] systemd[1]: Starting Create List of Static Device Nodes...
         Starting Create List of Static Device Nodes...
[    8.002272] systemd[1]: Starting Load Kernel Module configfs...
         Starting Load Kernel Module configfs...
[    8.022157] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
[    8.038323] systemd[1]: Starting Load Kernel Module fuse...
         Starting Load Kernel Module fuse...
[    8.055070] systemd[1]: Starting Start psplash boot splash screen...
         Starting Start psplash boot splash screen...
[    8.082570] fuse: init (API version 7.41)
[    8.090092] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    8.095668] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[    8.119953] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    8.150280] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    8.176890] systemd[1]: Starting Generate network units from Kernel command line...
         Starting Generate network units from Kernel co[    8.188665] systemd-journald[121]: Collecting audit messages is enabled.
mmand line...
[    8.201099] cryptodev: loading out-of-tree module taints kernel.
[    8.217777] sysctl table check failed: ioctl/(null) procname is null
[    8.225879] systemd[1]: Starting Remount Root and Kernel File Systems...
[    8.234000] sysctl table check failed: ioctl/(null) No proc_handler
         Starting Remount Root and Kernel File Systems   8.241730] cryptodev: driver 1.14 loaded.
[0m...
[    8.266123] systemd[1]: Starting Coldplug All udev Devices...
         Starting Coldplug All udev Devices...
[    8.297855] EXT4-fs (mmcblk1p2): re-mounted 0b4bc077-9173-4f02-9077-d360666c5df7 r/w. Quota mode: none.
[    8.302369] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    8.319094] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory /tmp.
[  OK  ] Finished Create List of Static Device Nodes.
[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Start psplas\E2temd progress communication helper.
[  OK  ] Finished Load Kernel Modules.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Remount Root and Kernel File Systems.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
         Starting Apply Kernel Variables...
[    8.655862] systemd-journald[121]: Received client request to flush runtime journal.
         Starting Create Static Device Nodes in /dev gracefully...
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Apply Kernel Variables.
[  OK  ] Finished Create Static Device Nodes in /dev gracefully.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /var/volatile...
[    8.871039] audit: type=1334 audit(1741187610.960:2): prog-id=6 op=LOAD
[    8.878010] audit: type=1334 audit(1741187610.968:3): prog-id=7 op=LOAD
         Starting Rule-based Manager for Device Events and Files...
[  OK  ] Mounted /var/volatile.
         Starting Load/Save OS Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create System Files and Directories...
[  OK  ] Finished Load/Save OS Random Seed.
[  OK  ] Finished Create System Files and Directories.
[    9.013071] audit: type=1334 audit(1741187611.100:4): prog-id=8 op=LOAD
         Starting Network Name Resolution...
[    9.055949] audit: type=1334 audit(1741187611.144:5): prog-id=9 op=LOAD
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[    9.109000] audit: type=1334 audit(1741187611.196:6): prog-id=10 op=LOAD
[    9.115765] audit: type=1334 audit(1741187611.208:7): prog-id=11 op=LOAD
[    9.123397] audit: type=1334 audit(1741187611.212:8): prog-id=12 op=LOAD
         Starting User Database Manager...
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[  OK  ] Started User Database Manager.
[  OK  ] Started Rule-based Manager for Device Events and Files.
[  OK  ] Found device /dev/ttyS2.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Time Set.
[  OK  ] Started Network Name Resolution.
[  OK  ] Reached target Host and Network Name Lookups.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily rotation of log files.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting Docker Socket for the API...
[  OK  ] Listening on dropbear.socket.
[  OK  ] Listening on PC/SC Smart Card Daemon Activation Socket.
[    9.657609] audit: type=1334 audit(1741230278.380:9): prog-id=13 op=LOAD
         Starting D-Bus System Message Bus...
         Starting Reboot and dump vmcore via kexec...
[  OK  ] Listening on Docker Socket for the API.
[  OK  ] Finished Reboot and dump vmcore via kexec.
[  OK  ] Reached target Socket Units.
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Reached target Basic System.
[  OK  ] Started Job spooling tools.
         Starting Avahi mDNS/DNS-SD Stack...
[  OK  ] Started Periodic Command Scheduler.
         Starting Print notice about GPLv3 packages...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
[  OK  ] Started irqbalance daemon.
[  OK  ] Started Multiple Spanning Tree Protocol Daemon.
         Starting Telephony service...
         Starting Expand the rootfs partiti\E2to full size of the boot device....
[  OK  ] Started strongSwan IPsec IKEv1/IKEv[   10.108434] audit: type=1334 audit(1741230278.832:10): prog-id=14 op=LOAD
2 daemon using ipsec.conf.
[   10.121660] audit: type=1334 audit(1741230278.848:11): prog-id=15 op=LOAD
         Starting User Login Management...
         Starting Telnet Server...
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[  OK  ] Reached target Preparation for Network.
         Starting Network Configuration...
[  OK  ] Finished Telnet Server.
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Started Telephony service.
[  OK  ] Started User Login Management.[   10.623561] Bluetooth: Core ver 2.22

[   10.631226] NET: Registered PF_BLUETOOTH protocol family
[   10.636724] Bluetooth: HCI device and connection manager initialized
[   10.643341] Bluetooth: HCI socket layer initialized
[   10.648467] Bluetooth: L2CAP socket layer initialized
[   10.653630] Bluetooth: SCO socket layer initialized
[   10.654690] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[  OK  ] Finished Expand the rootfs partition to full size of the boot device..
[   10.687781] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[   10.697937] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[  OK  ] Started Network Configuration.
[  OK  ] Reached target Network.
         Starting Enable and configure wl18xx bluetooth stack...
         Starting containerd container runtime...
         Starting LLDP daemon...
[  OK  ] Started Netperf Benchmark Server.
         Starting Simple Network Management Protocol (SNMP) Daemon....
         Starting Permit User Sessions...
[   10.902989] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[  OK  ] Finished Enable and configure wl18xx bluetooth stack.
[   10.958552] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[   10.968100] CAN device driver interface
[  OK  ] Finished Permit User Sessions.
[  OK  ] Started emptty display manager.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Reached target Login Prompts.
[   11.107687] mc: Linux media interface: v0.10
[   11.127258] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c
[   11.203893] PVR_K:  186: Device: 4e20000000.gpu
[  OK  ] Started LLDP daemon.
[   11.232160] videodev: Linux video capture interface: v2.00
[   11.234178] PVR_K:  186: Read BVNC 22.104.208.318 from HW device registers
[   11.268869] at24 0-0050: supply vcc not found, using dummy regulator
[   11.278109] PVR_K:  186: RGX Device registered with BVNC 22.104.208.318
[   11.285525] [drm] Initialized pvr 24.2.6643903 for 4e20000000.gpu on minor 0
[   11.305690] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[   11.446766] k3_r5_rproc bus@100000:bus@28380000:r5fss@41000000: k3_r5_cluster_rproc_init failed, ret = -517
[   11.465763] remoteproc remoteproc0: releasing 41000000.r5f
[   11.471785] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[   11.484110] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[   11.499621] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[   11.506401] platform 41000000.r5f: configured R5F for IPC-only mode
[   11.515652] platform 41000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
[   11.526734] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[   11.533408] remoteproc remoteproc0: 41000000.r5f is available
[   11.539262] remoteproc remoteproc0: attaching to 41000000.r5f
[   11.545364] rproc-virtio rproc-virtio.13.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
[   11.556138] virtio_rpmsg_bus virtio0: rpmsg host is online
[   11.561776] rproc-virtio rproc-virtio.13.auto: registered virtio0 (type 7)
[   11.564940] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[   11.570119] remoteproc remoteproc0: remote processor 41000000.r5f is now attached
[   11.575236] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[   11.590279] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[   11.602801] platform 5c00000.r5f: configured R5F for remoteproc mode
[   11.609361] platform 41400000.r5f: configured R5F for remoteproc mode
[   11.616233] img_enc 4200000.video-encoder: vxe_enc_probe: using heap 1 for internal alloc
[   11.631068] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[   11.631285] img_enc 4200000.video-encoder: encoder registered as /dev/video1
[   11.637734] platform 41400000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a1000000
[   11.657339] platform 5c00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
[   11.667427] remoteproc remoteproc2: 41400000.r5f is available
[   11.676367] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a9000000
[   11.696277] k3-dsp-rproc 4d80800000.dsp: configured DSP for remoteproc mode
[   11.704878] remoteproc remoteproc2: loading /lib/firmware/j7-mcu-r5f0_1-fw failed with error -22
[   11.717713] remoteproc remoteproc3: 4d80800000.dsp is available
[   11.725600] remoteproc remoteproc2: Direct firmware load for j7-mcu-r5f0_1-fw failed with error -22
[   11.741778] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a8000000
[   11.753609] remoteproc remoteproc2: powering up 41400000.r5f
[   11.761707] remoteproc remoteproc2: loading /lib/firmware/j7-mcu-r5f0_1-fw failed with error -22
[   11.775351] k3-dsp-rproc 4d81800000.dsp: configured DSP for remoteproc mode
[   11.786752] remoteproc remoteproc2: Direct firmware load for j7-mcu-r5f0_1-fw failed with error -22
[   11.797066] remoteproc remoteproc4: 4d81800000.dsp is available
[   11.797130] remoteproc remoteproc2: request_firmware failed: -22
[   11.805529] img_dec 4300000.video-decoder: decoder registered as /dev/video0
[   11.814767] k3-dsp-rproc 64800000.dsp: assigned reserved memory node vision-apps-c71-dma-memory@b2000000
[   11.825774] remoteproc remoteproc1: 5c00000.r5f is available
[   11.840940] k3-dsp-rproc 64800000.dsp: configured DSP for remoteproc mode
[   11.848214] platform 5d00000.r5f: configured R5F for remoteproc mode
[   11.848886] remoteproc remoteproc5: 64800000.dsp is available
[   11.866490] m_can_platform 40528000.can: m_can device registered (irq=840, version=32)
[   11.877484] platform 5d00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
[   11.888541] remoteproc remoteproc6: 5d00000.r5f is available
[   11.888619] m_can_platform 40568000.can: m_can device registered (irq=841, version=32)
[   11.922031] m_can_platform 2701000.can: m_can device registered (irq=842, version=32)
[   11.930234] remoteproc remoteproc4: powering up 4d81800000.dsp
[   11.940426] platform 5e00000.r5f: configured R5F for remoteproc mode
[   11.940916] remoteproc remoteproc4: Booting fw image j7-c66_1-fw, size 1018672
[   11.957028] m_can_platform 2721000.can: m_can device registered (irq=843, version=32)
[   11.957621] rproc-virtio rproc-virtio.14.auto: assigned reserved memory node vision-apps-c66-dma-memory@a8000000
[   11.965093] platform 5e00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a6000000
[   11.980262] virtio_rpmsg_bus virtio1: rpmsg host is online
[   11.984809] remoteproc remoteproc7: 5e00000.r5f is available
[   11.989630] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
[   11.995389] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[   12.006162] rproc-virtio rproc-virtio.14.auto: registered virtio1 (type 7)
[   12.011451] remoteproc remoteproc7: powering up 5e00000.r5f
[   12.018905] platform 5f00000.r5f: configured R5F for remoteproc mode
[   12.024038] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[   12.030197] remoteproc remoteproc4: remote processor 4d81800000.dsp is now up
[   12.039222] remoteproc remoteproc7: request_firmware failed: -2
[   12.048179] platform 5f00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a7000000
[   12.061875] remoteproc remoteproc8: 5f00000.r5f is available
[   12.068210] remoteproc remoteproc8: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[   12.077888] remoteproc remoteproc6: powering up 5d00000.r5f
[   12.080911] remoteproc remoteproc8: powering up 5f00000.r5f
[   12.084528] remoteproc remoteproc6: Booting fw image j7-main-r5f0_1-fw, size 351444
[   12.089962] remoteproc remoteproc8: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[   12.106065] remoteproc remoteproc3: powering up 4d80800000.dsp
[   12.112041] remoteproc remoteproc3: Booting fw image j7-c66_0-fw, size 1018672
[   12.119330] remoteproc remoteproc8: request_firmware failed: -2
[   12.126937] rproc-virtio rproc-virtio.15.auto: assigned reserved memory node vision-apps-c66-dma-memory@a9000000
[   12.138590] virtio_rpmsg_bus virtio2: rpmsg host is online
[   12.144107] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
[   12.151281] rproc-virtio rproc-virtio.15.auto: registered virtio2 (type 7)
[   12.158277] remoteproc remoteproc3: remote processor 4d80800000.dsp is now up
[   12.176939] remoteproc remoteproc1: powering up 5c00000.r5f
[   12.184725] remoteproc remoteproc1: Booting fw image j7-main-r5f0_0-fw, size 1711808
[   12.201798] rproc-virtio rproc-virtio.16.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
[   12.214060] rproc-virtio rproc-virtio.17.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
[   12.226080] virtio_rpmsg_bus virtio3: rpmsg host is online
[   12.232086] virtio_rpmsg_bus virtio4: rpmsg host is online
[   12.236593] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xd
[   12.237687] rproc-virtio rproc-virtio.16.auto: registered virtio3 (type 7)
[   12.251597] rproc-virtio rproc-virtio.17.auto: registered virtio4 (type 7)
[   12.258541] remoteproc remoteproc6: remote processor 5d00000.r5f is now up
[   12.265476] remoteproc remoteproc1: remote processor 5c00000.r5f is now up
[   12.364260] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled
[   12.374833] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled
[   12.385051] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled
[   12.395714] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled
[   12.407561] scsi host0: ufshcd
[   12.433199] remoteproc remoteproc9: b034000.pru is available
[   12.439751] remoteproc remoteproc10: b004000.rtu is available
[   12.444901] scsi 0:0:0:49488: Well-known LUN    TOSHIBA  THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[   12.454168] remoteproc remoteproc11: b00a000.txpru is available
[   12.461374] remoteproc remoteproc12: b038000.pru is available
[   12.467578] scsi 0:0:0:49476: Well-known LUN    TOSHIBA  THGAF8G8T23BAILB 0300 PQ: 0 ANSI: 6
[   12.467788] remoteproc remoteproc13: b006000.rtu is available
[   12.481852] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd
[   12.486544] remoteproc remoteproc14: b00c000.txpru is available
[   12.491494] cdns-ufshcd 4e84000.ufs: ufshcd_scsi_add_wlus: BOOT WLUN not found
[   12.495794] remoteproc remoteproc15: b134000.pru is available
[   12.508963] remoteproc remoteproc16: b104000.rtu is available
[   12.516640] remoteproc remoteproc17: b10a000.txpru is available
[   12.524144] remoteproc remoteproc18: b138000.pru is available
[   12.531696] remoteproc remoteproc19: b106000.rtu is available
[   12.538290] remoteproc remoteproc20: b10c000.txpru is available
[  OK  ] Created slice Slice /system/tee-supplicant.
[  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[  OK  ] Started TEE Supplicant on teepriv0.
         Starting Virtual Console Setup...
[   12.663269] m_can_platform 40528000.can mcu_mcan0: renamed from can0
[   12.674632] remoteproc remoteproc5: powering up 64800000.dsp
[   12.684761] remoteproc remoteproc5: Booting fw image j7-c71_0-fw, size 13234320
[   12.697035] remoteproc remoteproc5: unsupported resource 65538
[   12.707171] rproc-virtio rproc-virtio.18.auto: assigned reserved memory node vision-apps-c71-dma-memory@b2000000
[   12.707952] m_can_platform 40568000.can mcu_mcan1: renamed from can1
[   12.722052] virtio_rpmsg_bus virtio5: rpmsg host is online
[   12.730858] rproc-virtio rproc-virtio.18.auto: registered virtio5 (type 7)
[   12.740394] remoteproc remoteproc5: remote processor 64800000.dsp is now up
[   12.805721] m_can_platform 2721000.can main_mcan2: renamed from can3
[   12.853623] m_can_platform 2701000.can main_mcan0: renamed from can2
         Starting Save/Restore Sound Card State...
[  OK  ] Finished Save/Restore Sound Card State.
[  OK  ] Reached target Sound Card.
[  OK  ] Finished Virtual Console Setup.
[   13.278508] xhci-hcd xhci-hcd.19.auto: xHCI Host Controller
[   13.284164] xhci-hcd xhci-hcd.19.auto: new USB bus registered, assigned bus number 1
[   13.292038] xhci-hcd xhci-hcd.19.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000008010
[   13.301569] xhci-hcd xhci-hcd.19.auto: irq 868, io mem 0x06410000
[   13.307906] xhci-hcd xhci-hcd.19.auto: xHCI Host Controller
[   13.313501] xhci-hcd xhci-hcd.19.auto: new USB bus registered, assigned bus number 2
[   13.321248] xhci-hcd xhci-hcd.19.auto: Host supports USB 3.0 SuperSpeed
[   13.328307] hub 1-0:1.0: USB hub found
[   13.332141] hub 1-0:1.0: 1 port detected
[   13.336446] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[   13.344982] hub 2-0:1.0: USB hub found
[   13.348780] hub 2-0:1.0: 1 port detected
[   13.581583] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[   13.728927] hub 1-1:1.0: USB hub found
[   13.733018] hub 1-1:1.0: 4 ports detected
[   13.820468] usbcore: registered new device driver onboard-usb-dev
[  OK  ] Created slice Slice /system/systemd-fsck.
         Expecting device /dev/mmcblk1p1...
[  OK  ] Started Simple Network Management Protocol (SNMP) Daemon..
[  OK  ] Found device /dev/mmcblk1p1.
         Starting File System Check on /dev/mmcblk1p1...
[  OK  ] Finished File System Check on /dev/mmcblk1p1.
         Mounting /run/media/BOOT-mmcblk1p1...
[  OK  ] Mounted /run/media/BOOT-mmcblk1p1.
[  OK  ] Started containerd container runtime.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
	adwaita-icon-theme-symbolic
	autoconf
	bash-dev
	bash
	bc
	binutils
	cifs-utils
	coreutils-stdbuf
	coreutils
	cpio
	cpp-symlinks
	cpp
	dosfstools
	elfutils-dev
	elfutils
	findutils
	g++-symlinks
	g++
	gawk
	gcc-symlinks
	gcc
	gdb
	gdbserver
	gettext
	glmark2
	gnu-config
	grub-common
	grub-editenv
	grub-efi
	gzip
	hidapi
	kbd-dev
	kbd-keymaps-pine
	less
	libasm1
	libatomic-dev
	libatomic1
	libbfd
	libdebuginfod1
	libdw1
	libelf1
	libgcc-s-dev
	libgcc1
	libgdbm-compat4
	libgdbm-dev
	libgdbm6
	libgettextlib
	libgettextsrc
	libgmp-dev
	libgmp10
	libgmpxx4
	libgnutls-dev
	libgnutls-openssl27
	libgomp1
	libidn2-0
	libidn2-dev
	libmpc3
	libmpfr6
	libopcodes
	libqt6shadertools-dev
	libqt6shadertools-plugins
	libqt6shadertools-qmlplugins
	libqt6shadertools6
	libreadline-dev
	libreadline8
	libstdc++-dev
	libstdc++6
	libtasn1-dev
	libunistring-dev
	libunistring5
	m4
	make
	nettle-dev
	nettle
	parted
	piglit
	qtbase-dev
	qtbase-examples
	qtbase-plugins
	qtbase-qmlplugins
	qtbase-staticdev
	qtbase
	qtdeclarative-dev
	qtdeclarative-plugins
	qtdeclarative-qmlplugins
	qtdeclarative-staticdev
	qtdeclarative
	qtlanguageserver-dev
	qtlanguageserver-plugins
	qtlanguageserver-qmlplugins
	qtlanguageserver-staticdev
	qtlanguageserver
	qtsvg-dev
	qtsvg-plugins
	qtsvg-qmlplugins
	qtsvg
	qtwayland-dev
	qtwayland-plugins
	qtwayland-qmlplugins
	qtwayland
	tar
	which

If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************

 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project j721e-evm ttyS2

Arago 2025.01 j721e-evm ttyS2

j721e-evm login: [   17.164436] kauditd_printk_skb: 2 callbacks suppressed
[   17.164445] audit: type=1006 audit(1741230285.888:14): pid=1036 uid=0 subj=kernel old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
[   17.183372] audit: type=1300 audit(1741230285.888:14): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffda3af218 a2=4 a3=1 items=0 ppid=1 pid=1036 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
[   17.211280] audit: type=1327 audit(1741230285.888:14): proctitle="(systemd)"

j721e-evm login: root
[   23.857346] audit: type=1006 audit(1741230292.580:15): pid=1049 uid=0 subj=kernel old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=2 res=1
[   23.871099] audit: type=1300 audit(1741230292.580:15): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffef122a58 a2=1 a3=1 items=0 ppid=1 pid=1049 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=2 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
[   23.874976] platform connector: deferred probe pending: platform: supplier regulator-dp-pwr not ready
[   23.898775] audit: type=1327 audit(1741230292.580:15): proctitle="(systemd)"
[   23.908812] platform regulator-dp-pwr: deferred probe pending: reg-fixed-voltage: can't get GPIO
[   23.924413] audit: type=1334 audit(1741230292.652:16): prog-id=18 op=LOAD
[   23.931509] audit: type=1300 audit(1741230292.652:16): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffd0fdf708 a2=90 a3=0 items=0 ppid=1 pid=1049 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=2 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
[   23.958370] audit: type=1327 audit(1741230292.652:16): proctitle="(systemd)"
[   23.965480] audit: type=1334 audit(1741230292.652:17): prog-id=18 op=UNLOAD
[   23.972498] audit: type=1300 audit(1741230292.652:17): arch=c00000b7 syscall=57 success=yes exit=0 a0=8 a1=1 a2=0 a3=ffff81193c60 items=0 ppid=1 pid=1049 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=2 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
[   23.999371] audit: type=1327 audit(1741230292.652:17): proctitle="(systemd)"
[   24.006667] audit: type=1334 audit(1741230292.652:18): prog-id=19 op=LOAD
root@j721e-evm:~# 
root@j721e-evm:~# ls
J721E_bootlogs.txt
root@j721e-evm:~#