Part Number: AM6422
Tool/software:
Hello,
We are currently utilizing the R5F for development, employing its internal ADC for sampling. Data is acquired in continuous mode and stored in a double - buffer configuration via DMA. For instance, when operating at a sampling rate of 100K, we set the DMA transfer count to generate an event interrupt. The interrupt occurs every 100 sampling points, which translates to an event interrupt once every 1ms. Once the first interrupt is triggered, the ADC can continue functioning normally and store data in the second buffer, thus avoiding data overwriting. The examples provided mostly focus on single - shot sampling and offer limited information on the integration with DMA. We would greatly appreciate it if you could offer some guidance to help us develop the functionality we've mentioned. Thank you very much.