Part Number: TDA4VH-Q1
Tool/software:
As per tiovx documentation,
It is not recommended to use vx_delay objects when using pipelining with TIOVX. The delay objects will unintentionally create serializations in the graph and break the desired pipelining.
Instead of using delay objects, graph parameters can be used to emulate a delay in the graph, thus allowing the delay to be handled in the application.