Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
After upgrading the AM62x SDK from 09.02.01.09 to 11.00.09.04, the error is occurred in OPTEE.
U-Boot SPL 2025.01-00406-gcd91d7360181-dirty (Mar 25 2025 - 16:14:37 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
Changed A53 CPU frequency to 1000000000Hz (S grade) in DT
SPL initial stack usage: 13424 bytes
Trying to boot from MMC2
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Starting ATF on ARM64 core...
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_do_xfer:120 Message receive failed (-65523)
E/TC:0 0 ti_sci_init:480 Unable to communicate with control firmware (-65523)
E/TC:0 0 do_init_calls:22 early_initcall __text_start + 0x000727e8 failed
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_do_xfer:120 Message receive failed (-65523)
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_do_xfer:120 Message receive failed (-65523)
E/TC:0 0 sa2ul_init:106 Could not change TRNG firewall owner
E/TC:0 0 do_init_calls:22 service_initcall __text_start + 0x00072b50 failed
Could you tell me the workaround?
Best Regards,
Koji