Other Parts Discussed in Thread: OMAPL138
Hi,
I am working on TWO AIC3106 codecs which using the McASP and McBSP1 port for C6748 processor (OMAPL138 board) for two independent audio channel processing.
McASP work fine from the PSP package examples given under audiosample, however the McBSP1 (original from PSP's mcbspSampleSlave examples) wasn't when interfacing with another AIC31 codec, the CPU loading always high and keep pooling at Mcbsp_swiTxFifo() when tracing. This cause the output audio quality distortion.
I will be very appreciate if anyone who can provide me with a example for McBSP1 interface with AIC31 codec or its configuration with the TI codec.
Here my current McBSP1 configuration:
////////////////////////////////
/**< settings to configure the TX or RX hardware sections */
Mcbsp_DataConfig mcbspTxChanConfig =
{
Mcbsp_Phase_SINGLE,
Mcbsp_WordLength_32,
Mcbsp_WordLength_32, /* Dont care for single phase*/
NUM_OF_CHANNELS,
NUM_OF_CHANNELS, /* Dont care for single phase*/
Mcbsp_FrmSync_DETECT,
Mcbsp_DataDelay_0_BIT,
Mcbsp_Compand_OFF_MSB_FIRST,
Mcbsp_BitReversal_DISABLE,
Mcbsp_IntMode_ON_READY,
Mcbsp_RxJust_RZF, /* Dont care for TX */
Mcbsp_DxEna_OFF
};
/**< settings to configure the TX or RX hardware sections */
Mcbsp_DataConfig mcbspRxChanConfig =
{
Mcbsp_Phase_SINGLE,
Mcbsp_WordLength_32,
Mcbsp_WordLength_32, /* Dont care */
NUM_OF_CHANNELS,
NUM_OF_CHANNELS, /* Dont care */
Mcbsp_FrmSync_DETECT,
Mcbsp_DataDelay_0_BIT,
Mcbsp_Compand_OFF_MSB_FIRST,
Mcbsp_BitReversal_DISABLE,
Mcbsp_IntMode_ON_READY,
Mcbsp_RxJust_RZF, /* Dont care for TX */
Mcbsp_DxEna_OFF
};
/**< clock setup for the TX section */
Mcbsp_ClkSetup mcbspTxClkConfig =
{
Mcbsp_FsClkMode_EXTERNAL,//Mcbsp_FsClkMode_INTERNAL, /* internal clock for master */
MCBSP_SAMPLE_RATE, /* 8KHz */
Mcbsp_TxRxClkMode_EXTERNAL,//Mcbsp_TxRxClkMode_INTERNAL,
Mcbsp_FsPol_ACTIVE_HIGH,
Mcbsp_ClkPol_RISING_EDGE
};
/**< clock setup for the RX or the TX section */
Mcbsp_ClkSetup mcbspRxClkConfig =
{
Mcbsp_FsClkMode_EXTERNAL,
MCBSP_SAMPLE_RATE, /* 8KHz */
Mcbsp_TxRxClkMode_EXTERNAL,
Mcbsp_FsPol_ACTIVE_HIGH,
Mcbsp_ClkPol_RISING_EDGE,
};
/**< Multi channel setup */
Mcbsp_McrSetup mcbspTxMultiChanCtrl =
{
Mcbsp_McmMode_ALL_CHAN_ENABLED_UNMASKED,
Mcbsp_PartitionMode_CHAN_0_15,
Mcbsp_PartitionMode_CHAN_16_31,
Mcbsp_PartitionMode_2
};
/**< Multi channel setup */
Mcbsp_McrSetup mcbspRxMultiChanCtrl =
{
Mcbsp_McmMode_ALL_CHAN_ENABLED_UNMASKED,
Mcbsp_PartitionMode_CHAN_0_15,
Mcbsp_PartitionMode_CHAN_16_31,
Mcbsp_PartitionMode_2
};
Mcbsp_ChanParams mcbspTxChanparam =
{
Mcbsp_WordLength_32, /* wordlength configured */
NULL, /* loop job buffer internal */
0, /* user loopjob length */
NULL, /* global error callback */
NULL, /* edma Handle */
(0u), /* EDMA event queue */
10,/*8,*/ /* hwi number */
Mcbsp_BufferFormat_1SLOT,
TRUE, /* FIFO mode enabled */
&mcbspTxChanConfig, /* channel configuration */
&mcbspTxClkConfig, /* clock configuration */
&mcbspTxMultiChanCtrl, /* multi channel control */
0x00,
0x00,
0x00,
0x00
};
Mcbsp_ChanParams mcbspRxChanparam =
{
Mcbsp_WordLength_32, /* wordlength configured */
NULL, /* loop job buffer internal */
0, /* user loopjob length */
NULL, /* global error callback */
NULL, /* edma Handle */
(1u), /* EDMA event queue */
9, /* hwi number */
Mcbsp_BufferFormat_1SLOT,
TRUE, /* FIFO mode enabled */
&mcbspRxChanConfig, /* channel configuration */
&mcbspRxClkConfig, /* clock configuration */
&mcbspRxMultiChanCtrl, /* multi channel control */
0x00,
0x00,
0x00,
0x00
};
///////////////////////////////////////////////
Thanks in advance,
PST