Part Number: SK-AM62A-LP
Tool/software:
Hi, I have followed the steps exactly as described in the Quick Start Guide
And I get the following output upon boot:
U-Boot SPL 2024.04-ti-g29d0c23d67ee (Nov 29 2024 - 11:41:54 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)') SPL initial stack usage: 13568 bytes Trying to boot from MMC2 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty NOTICE: BL31: Built : 04:20:32, Nov 1 2024 U-Boot SPL 2024.04-ti-g29d0c23d67ee (Nov 29 2024 - 11:41:54 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)') Trying to boot from MMC2 am654_sdhci mmc@fa00000: No passing ITAPDLY, return 0 Partition 1 invalid on device 1 spl_register_fat_device: fat register err - -1 spl_load_image_fat: error reading image u-boot.img, err - -1 SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
What might be the issue? One thing I noticed is that it says it is trying to boot from MMC2, but on the SK-AM62A-LP AM62A Low-Power SK EVM User’s Guide (Rev. A) that the microSD card corresponds with MMC1. Is this the issue? I have confirmed that my boot mode switches are in the proper position as well.
Thanks!