Part Number: TDA4VM
Other Parts Discussed in Thread: DS90UB960-Q1EVM
Tool/software:
Hi TI team,
I’m working on a 4-camera input project using the SK-TDA4VM EVM, and I would like to connect up to 4 FPD-Link III cameras—possibly IMX390 modules with UB953 serializers.
I’ve reviewed TI documentation and believe the DS90UB960-Q1EVM might be a good candidate as a deserializer, since it supports multiple FPD-Link inputs and MIPI CSI-2 output.
Could you help confirm:
1. Is the DS90UB960-Q1EVM officially compatible with SK-TDA4VM?
2. Is it possible to connect the DS90UB960-Q1EVM directly to J24 on the SK-TDA4VM and use all 4 camera inputs simultaneously through this single deserializer board?
3. Does TI provide any sample device trees, reference software, or EdgeAI PSDK support for using the UB960 board with SK-TDA4VM?
Any guidance on recommended deserializer boards for this setup would be greatly appreciated.
Thanks!