This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Playback of multiple video stream for PIP kind of application

Other Parts Discussed in Thread: DM3730

Hi,

 

Is it possible to playback multiple H264 streams (max 3) and display it on DVI with DM3730 using either the DVSDK sample applications or gstreamer?

 

Regards,

Amol

  • Amol,

             You have to write your own application for this. you can use decode sample application for this, I think OMTB has the feature to decode multiple video streams but not it can display.

             I think you need to ensure below capabilities.

             - Decode capability, depending on your stream resolutions it might be possible to decode 3 streams, watch for DSP load on the display.

             - Belnding the 3 channel to single frame to display to DVI, I am not sure if hardware supports blending, otherwise you need to have software blending which might load ARM.

            Refer to http://processors.wiki.ti.com/index.php/UserGuideDisplayDrivers_PSP_04.02.00.07 to know display driver capability. Refer to doc as per your PSP.

    Best Regards,

    Velan