This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reaching PCISTATSET (C6455)

Hello Gents,

I am trying to reach PCISTATSET from our PCI host. It sounds like I should map 0x02C00000 to one of the BAR using the translation registers and these registers are available in the backend registers also. It sounds a bit like the chicken and the egg.  Does it means it is mandatory to have a DSP software modifying these registers and then we can do PCI boot or is there anything I can do. I was hoping everything was achievable from the host side. The default translation is as the following:

 

BAR0    :   0x00080000 (8MB)

BAR1    :   0x00180000 (4MB)

BAR2    :   0x00280000 (8MB)

BAR3    :   0x08000000 (8MB)

BAR4    :   0x0A000000 (8MB)

BAR5    :   0x0E000000 (8MB)

So if my understanding is correct there are no way to typically send a DSPINT via PCISTATSET unless the DSP as previously mapped the 0x02C00000 to maybe BAR3.

Any ideas/comments are welcome of course,

Thanks!

Arnaud