This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: TMDSEMU560V2STM-U - XDS560V2 SYSTEM TRACE CONNECTOR

Other Parts Discussed in Thread: TMDSEMU560V2STM-U

Tool/software:

Hi Team,

We are planning to use TMDSEMU560V2STM-U Emulator for our customer requirement. I understand Emulator end has QSH series connector. So, Can I use QTH-030-01-L-D-A in my custom board?

Regards,

Srikanth Kacchu

  • Are you planning to use the parallel trace buffer function in the debugger to capture trace data? I'm asking because we find very few customers are designing a system that allows the 26 pins associated with parallel trace to be reserved for this function. Most customers decide to use the much smaller internal trace buffer and export the data at a much slower rate via the JTAG scan pins. If so, you are more like going to use the 60-pin to 14-pin or 20-pin adapter for connecting to your system, where you only need to implement a 14-pin or 20-pin header for connecting the debugger.

    You will need to contact Blackhawk if you still need to know the answer to this question. Blackhawk makes the debugger for TI. They should be able to provide support for these types of questions. https://www.blackhawk-dsp.com/

    Regards,
    Paul