Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi
I have a problem to upload custom software or TI examples from SDK to other R5 cores than R5_0 core 0. Attempt to flash example software e.g empty_am64x-evm_r5fss0-1_nortos_ti-arm-clang and with error:
MAIN_Cortex_R5_0_1: Error connecting to the target: (Error -6305) PRSC module failed to write to a router register. (Emulation package 20.2.0.3536)
And this happens also when I try to flash empty project on any other core besides R5_0 core 0 - on that core everything works fine.
We are using:
- CCS 20.2.0.12__1.8.0
- MCU + SDK for AM64x 10.1.0.32
- SysConfig 1.23.0
- XDS110 Debug Probe Rev. A
Based on related topics I tried to use older version of software CCS, MCU+SDK and SysConfig and also lowering the TCLK JTAG speed. It does not help.
Thanks for help.
BR
Jakub