This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

boot fail after update filesystem on nand flash

i update filesystem on nand flash(jffs2), but the board boot fail, does anyone have any idea ?

following are the boot log.

TI8148_IPNC#printenv
bootdelay=3
baudrate=115200
autoload=yes
verify=yes
ramdisk_file=ramdisk.gz
loadaddr=0x81000000
script_addr=0x80900000
loadbootscript=fatload mmc 1 ${script_addr} boot.scr
bootscript= echo Running bootscript from MMC/SD to set the ENV...; source ${script_addr}
ethact=cpsw
filesize=1E1E524
fileaddr=81000000
bootcmd=nboot 0x81000000 0 0x280000; bootm
bootfile=uImage_ipnc_dm81xx
ethaddr=00:0C:0C:A0:FF:FA
ipaddr=192.168.2.167
serverip=192.168.2.166
bootargs=mem=80M vram=4M notifyk.vpssm3_sva=0xBFD00000 console=ttyO0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 ip=192.168.2.167:192.168.2.166:192.168.0.1:255.255.248.0:dm812x_ipnc:eth0:off eth=00:0C:0C:A0:FF:FA earlyprintk
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2010.06 (Nov 11 2011 - 14:38:45) DM814x-IPNC-1.5.0
Environment size: 791/8188 bytes
TI8148_IPNC#boot
Loading from nand0, offset 0x280000
   Image Name:   Linux-2.6.37_IPNC_DM812x_1.5.0
   Created:      2011-11-11   6:41:29 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2228500 Bytes = 2.1 MiB
   Load Address: 80008000
   Entry Point:  80008000
## Booting kernel from Legacy Image at 81000000 ...
   Image Name:   Linux-2.6.37_IPNC_DM812x_1.5.0
   Created:      2011-11-11   6:41:29 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2228500 Bytes = 2.1 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37_IPNC_DM812x_1.5.0 (root@ubuntu) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #2 Fri Nov 11 14:41:22 CST 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8148ipnc
vram size = 4194304 at 0
bootconsole [earlycon0] enabled
reserved size = 4194304 at 0
FB: Reserving 4194304 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8148 1.0
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 19296
Kernel command line: mem=80M vram=4M notifyk.vpssm3_sva=0xBFD00000 console=ttyO0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 ip=192.168.2.167:192.168.2.166:192.168.0.1:255.255.248.0:dm812x_ipnc:eth0:off eth=00:0C:0C:A0:FF:FA earlyprintk
cpsw: kernel boot params Ethernet address: 00:0C:0C:A0:FF:FA
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 76MB = 76MB total
Memory: 72256k/72256k available, 9664k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xffc00000 - 0xffe00000   (   2 MB)
    vmalloc : 0xc5800000 - 0xf8000000   ( 808 MB)
    lowmem  : 0xc0000000 - 0xc5000000   (  80 MB)
    modules : 0xbf000000 - 0xc0000000   (  16 MB)
      .init : 0xc0008000 - 0xc0035000   ( 180 kB)
      .text : 0xc0035000 - 0xc043b000   (4120 kB)
      .data : 0xc043c000 - 0xc0477740   ( 238 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:375
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ368
Trying to install interrupt handler for IRQ369
Trying to install interrupt handler for IRQ370
Trying to install interrupt handler for IRQ371
Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ374
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
OMAP clockevent source: GPTIMER1 at 20000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy: 
NET: Registered protocol family 16
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 4
registered ti814x_vpss device
registered TI814x on-chip HDMI device
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
PWM0 init success.
PWM1 init success.
bio: create slab <bio-0> at 0
SCSI subsystem initialized
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, peripheral, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
musb-hdrc musb-hdrc.0: USB Peripheral mode controller at c580c000 using DMA, IRQ 18
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 141
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled, bootconsole disabled
console [ttyO0] enabled, bootconsole disabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
brd: module loaded
loop: module loaded
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron )
Creating 6 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "U-Boot-min"
0x000000020000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffffd
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
mice: PS/2 mouse device common for all mice
rtc-tps65911 1-002d: rtc core: registered rtc-tps65911 as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbfd00000
tlv320aic26-codec 1-0000: Probing AIC26 SoC CODEC driver
asoc: tlv320aic26-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
  #0: TI8148 IPNC
TCP cubic registered
NET: Registered protocol family 17
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
rtc-tps65911 1-002d: setting system clock to 2000-01-01 06:16:46 UTC (946707406)
CPSW phy found : id is : 0x282f014
IP-Config: Complete:
     device=eth0, addr=192.168.2.167, mask=255.255.248.0, gw=192.168.0.1,
     host=dm812x_ipnc, domain=, nis-domain=(none),
     bootserver=192.168.2.166, rootserver=192.168.2.166, rootpath=
VFS: Mounted root (jffs2 filesystem) on device 31:4.
devtmpfs: error mounting -2
Freeing init memory: 180K
Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
Backtrace: 
[<c0043b44>] (dump_backtrace+0x0/0x110) from [<c032a24c>] (dump_stack+0x18/0x1c)
 r7:00000013 r6:c006663c r5:c0008670 r4:c0477e50
[<c032a234>] (dump_stack+0x0/0x1c) from [<c032a2b0>] (panic+0x60/0x17c)
[<c032a250>] (panic+0x0/0x17c) from [<c0035574>] (init_post+0xa4/0xc4)
 r3:c461af00 r2:00000000 r1:c053a340 r0:c03d247d
[<c00354d0>] (init_post+0x0/0xc4) from [<c0008788>] (kernel_init+0x118/0x154)
 r5:c0008670 r4:c0477740
[<c0008670>] (kernel_init+0x0/0x154) from [<c006663c>] (do_exit+0x0/0x5e4)
 r5:c0008670 r4:00000000