Other Parts Discussed in Thread: J7EXPA01EVM
Tool/software:
Dear Support team,
Currenty we are acquired the two of J784S4XG01EVM EVM. By using the provide SD card with sample application for HW functional testing, here we encounter two issues.
Test Procedure
A. Installation the fusion board (J7EXPA01EVM) with J784S4XG01EVM
B. Connect the D3 camera with fusion board via Fakra cable
C. Connect the Micro USB UART cable to J784S4XG01EVM
D. Connect DP to the monitor
E. Insert the provided test SD card
F. Open the minicom from PC
G. Connect the Power supply and Power ON the J784S4XG01EVM
H. Use root to Login
I. Run the sample application ./run_app_multi_cam.sh within /opt/vision_apps directory
J. The 4 camera views shows on monitor
Issue symptom
1. J784S4 reboot after 10 mins without any error log from UART console (the two EVM boards had the same issue)
2. The UART port was disconnected randomly (approximately 2-3 mins). On of the EVM board with this issue.
Please help!
BR,
Winner