This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to setup when using TVP5158 to DM3730

Other Parts Discussed in Thread: TVP5158, DM3730

Hi,

We needs add 3-ch D1 to DM3730 via TVP5158, BT.656 format, but connection error.

When using 2-ch D1 input with TVP5158, DM3730 can get VD0 interrupt (omap34xx_isp_isr()), then DM3730 can process data, it's working normal. NOW PCLK=54Mhz

Same setup, only change input channel to 3-ch, DM3730 could not get VD0, now PCLK=81Mhz

Besides, in DM3730 datasheet, the MAXIAM PCLK of BT.656 is 75Mhz.

 

So the question is: Can DM3730 can support 3-ch D1 input with TVP5158/BT.656/81Mhz? if Yes, how to setup it?

It is very urgent for product design, please help to check it.

Thanks a lot!