i have installed minicom and i am at the process of ......,
i have seen arago project in terminal and i got as follows:
root@dm3730-am3715:/ like this i got
and here i have given ifup eth0 then it showed already registered.
then i have given ifconfig then it showed as below:
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
it has not given the target ip address.
how could i find out it....?