Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello TI support team.
The SDK is mcu_plus_sdk_am64x_08_06_00_45.
I have two questions about watchdog_interrupt_am64x-sk_r5fss0-0_nortos_ti-arm-clang.
- Q1.
In the sysconfig of the above example, "WDT Reset Mode" was changed from "trigger NMI interrupt" to "trigger warm reset".
I was expecting a reset after 1000ms.
I built it, loaded it into CR5 and ran it from RAM, but it didn't reset.
Do I need to modify watchdog_interrupt_mode.c ?
- Q2.
Also, when "WDT Reset Mode" was set to "trigger NMI interrupt",
I changed "WDT Expiry Time in Millisecond (ms)" from 1000 to 1, but the NMI interrupt(watchdogCallback) did not occur correctly.
What could be the cause of this ?
Best regards,
Kiyomasa Imaizumi.