Part Number: AM6442
Other Parts Discussed in Thread: TMDS64EVM
Tool/software:
We are currently working with the TMDS64EVM to make custom board with AM644 and interfacing it with the XDS560v2-USB Emulator from Blackhawk. We noticed that the MIPI connector pinout on the TMDS64EVM differs from the pinout information shared by Blackhawk for the emulator cable (part number SQCD-025-12.00-STR-TEU-1).
Could you please confirm the following:
1. Is the MIPI connector on the TMDS64EVM designed to be directly compatible with the XDS560v2 emulator cable?
2. If not, do you recommend any adapter or cable configuration to enable proper connection between the two?
3. Is there a reference document or guideline for the expected pinout or mapping for the MIPI60 connector on the EVM?