This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: The Need for OSC1

Part Number: AM5708


Tool/software:

I plan to connect OSC0 to 20MHz and it will work.

I don't really understand the cases in which OSC1 is necessary.

Basically, is it okay not to connect it if I'm not using the MCASP function?

Hiroshi Yamada