This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6422: Run secured tiboot3.bin from the kernel.

Part Number: AM6422


Tool/software:

Hello Team,

In our custom board, we are using TI AM64x processor with the secure boot enable and we are using only eMMC as boot option(disable backup boot option).

Can we boot into the kernel (non-secure image), send tiboot3.bin to the R5/M4 core over RPC, and force it to run? We are checking to modify the tiboot3.bin(TI OTP tool) for changing the boot partition after the key burn. So when we boot next time from the second partition (under discussion).

Will it work? if yes, then provide the steps; if not, suggest an alternative strategy.

Thanks

Dharmik