Tool/software:
Hi TI,
When looking at the CPSW0 registers for policers, I noticed that there seems to be 2 tables : one for policing entries and one for classifiers that allows packet steering to particular thread IDs.
Furthermore, the CSL functions to set policing entries put the same index in both tables.
Questions are the following:
- Can I independently write into the classifiers table without creating a corresponding policing entry ?
- If i created a classifier entry N for a corresponding policing entry N, is it possible to use the classifier entry N in another policing entry N+M ?
- Essentially, can a same classifier be used for different policing entries or will I have to create duplicate classifiers for different policing entries ?
Thanks in advance for your time and answer.
Best regards