This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM67: AM67x SDK 11 watchdog can't setup timeout

Part Number: AM67


Tool/software:

Hi,

I want to setup rti_wdt watchdog timeout, but it is 60s also, it can't change. how to modify the watchdog timeout?

|TEST START|wdt_tests|
|TRACE LOG|******** WDT Testcase parameters ******** |
|TRACE LOG|Device : /dev/watchdog0|
|TRACE LOG|Loop Count : 1|
|TRACE LOG|Operation : Ioctl|
|TRACE LOG|Ioctl Name : WDIOC_SETTIMEOUT|
|TRACE LOG|Ioctl Arg : 60 |
|TRACE LOG| ************* End of Test params ************* |
IOCTL FAILED: Operation not supported
|TEST RESULT|FAIL|wdt_tests|