I can successfully run the pre-built starterware examples. When I try to build them and run the ones I built, the graphics are messed up. The example I am mainly interested in is the usb-dev-msc. It shows the blue bars at the top and bottom with the white text, but the middle of the screen is just mostly white random gibberish. More importantly, Windows doesn't even see the external usb drive when I plug the device into my PC.
I have tried these compilers:
IAR
gcc from code sourcery
CCS with CGT (the application doesn't even startup)
I am using the am1808 eval board from logic PD and the sfh_OMAP-L138.exe flashing tool.
Any ideas on what I am missing?