Part Number: TDA4VM
Tool/software:
In TDA4, for TIDL use case applications,
1. Do we have control to change / schedule the tasks running on "C7x" meant for MMA processing
2. If yes, pls point out the source code files under SDK and the related docs if any
3. when i run app_tidl_od for the yuv files included in SDK, i observe the detection timing is in range of 100ms to 500ms or more. As per TI, what is the average time taken for detecting the vehicle, lets say, to be used under FCW (Forward collision warning) using tidl_od model supplied in SDK.